Avnet Abacus reveals details of cooperation to save millions of smart meters from landfill
Distributor helps TWTG develop upgraded wireless communications module integrating advanced battery technology from Nichicon for automatic electricity meter reading applications
Brussels, Belgium, 30th November, 2022: Avnet Abacus, one of Europe’s leading distributor of interconnect, passive, electromechanical, power supply, energy storage, wireless & sensor products and a regional business unit of Avnet (NASDAQ: AVT), has unveiled details of its recent cooperation with TWTG, a leading industrial-IoT specialist based in Rotterdam, helping to prevent the disposal of millions of smart meters. Key to the collaboration was the integration of advanced battery technology from leading manufacturer Nichicon into a new wireless communications module.
The viability of existing smart meters – which originally sent their data via 2G/GPRS – is subject to the inevitable progress of technology. Voice and data services are increasingly being delivered over 3G/4G and eventually 5G networks, as well as other technologies such as LPWAN, including LTE Cat-M1, NB-IoT and LoRa. The shutdown of older network technologies creates a major problem for utility companies. It threatens the necessary replacement of smart meters – which could end up in landfill – and mean high costs to install new meters.
One leading European provider delivering smart-metered electricity to one and a half million households and businesses faced this very problem. It turned to TWTG to design a retrofit module to work with their installed base of smart meters and communicate with the outside world using the LTE-M.
A key pathway to the new module was use of the smart meter’s P1 access port – used for various purposes from firmware upgrades to device monitoring. However, the port offers a small output of approximately 5mA, which is not enough to send a message via 4G. The design would therefore require a small, yet powerful, energy storage device to acquire energy from the port, store it and deliver enough power to the module to send data via LTEM.
Avnet Abacus was called in to help source the energy storage device and provide support for the new module’s design. Options considered included a supercapacitor – but its lower energy density meant it would have been too large for the required compact design. Additionally, it was crucial that the battery would last for 10 to 15 years, meeting all the challenges of being charged and discharged without failure over for an extended period; and exceeding national government regulations, so the module could potentially be deployed across Europe.
Avnet Abacus came up with the solution in the form of an innovative battery from Nichicon, which had developed a battery for use in a stylus pen for a consumer-market mobile phone. Connecting via Bluetooth, the Nichicon SLB series battery could be charged quickly via wireless charging within a few minutes, plus it was built to last thousands of charge/discharge cycles. The SLB battery was able to accumulate enough charge from the 5mA P1 output to power a single data message per day. In addition to the battery, the prototype retrofit module included an advanced multi-mode LPWAN module supporting LTE Cat-M1, Kyocera-AVX antenna, Molex connectors and a SIM card.
“We were really impressed with the support from the Avnet Abacus team and their innovative solution,” said Wesley Kerstens, Hardware Lead at TWTG. “Their help and the selection of the Nichicon battery technology in particular helped us meet all the necessary requirements in a simple and compact package.”
According to Marc Eichhorn, Product Manager Batteries at Avnet Abacus: “There is great potential to deploy Nichicon’s SLB series technology in a host of remote devices in IoT applications, or as a potential replacement for non-rechargeable batteries in next-generation product designs using energy harvesting from small solar cells. It also means that the battery is no longer the life-limiting factor of products.”
A video on the case study is available at:
www.avnet.com/abacus/manufacturers/m/nichicon/
Further information on the Nichicon battery is available at:
www.avnet.com/abacus/products/new-products/npi/nichicon-slb-series/
About Avnet Abacus
Avnet Abacus is a pan-European distributor committed to supporting customers from design to fulfilment. Avnet Abacus’ exceptional linecard features globally recognized manufacturers and an extensive product range that includes interconnect, passive, electromechanical, power supply, energy storage, wireless & sensor products and solutions. Avnet Abacus is a regional business unit of Avnet, (NASDAQ:AVT), with European headquarters in Belgium (Avnet Europe BV). For more information, visit: www.avnet-abacus.eu or follow us on http://www.twitter.com/Avnet_Abacus.
About Avnet
Avnet is a global technology solutions provider with an extensive ecosystem delivering design, product, marketing and supply chain expertise for customers at every stage of the product lifecycle. We transform ideas into intelligent solutions, reducing the time, cost and complexities of bringing products to market. For nearly a century, Avnet has helped its customers and suppliers around the world realize the transformative possibilities of technology. Learn more about Avnet at www.avnet.com.
Legal Disclaimer:
All brands and trade names are trademarks or registered trademarks, and are the properties of their respective owners. Avnet disclaims any proprietary interest in marks other than its own.
For further information:
Anja Woithe - Senior PR Manager Avnet EMEA
Im Technologiepark 2-8
D-85586 Poing
E: anja.woithe@avnet.eu
T: +49.8121.774.459
Latest news from Avnet Abacus
Keep up-to-date with the latest company news and announcements
Learn MoreEngineers' Insight
Helping to solve design challenges
READ THE BLOGFocus Magazine
Featuring in-depth trend and technology reviews, and new product spotlights, Focus keeps you up to speed with the fastest moving industry in the world.
READ MORE