Design Trends: Batteries For Iot | Avnet Abacus
Design Trends: Batteries For Iot | Avnet Abacus

Design trends: Batteries for IoT

Tim Parker Photo

Selecting batteries for Internet of Things connected systems can be tricky, as there is such a wide variety of application types.

The Internet of Things phenomenon is allowing the collection of data from sensor nodes practically anywhere in the environment, and giving non-electronic objects the ability to communicate, opening up a whole new sphere of applications for electronic systems. Selecting batteries for Internet of Things connected systems can be tricky, as there is such a wide variety of application types. 

For the ubiquitous sensor node at the periphery of the Internet of Things – things like thermostats, building automation sensors and light switches – this type of system has a very specific power profile. The application will typically be in sleep mode for the vast majority of the time, waking up only to perform a measurement, or to activate a low power wireless connection such as Bluetooth Low Energy. When in sleep mode, the device consumes a very small amount of power, but when active, a burst of power is required. These devices are very low power overall because the sleep period is generally many orders of magnitude longer than the active period.

These types of applications typically use coin cell batteries because of their low overall power requirement. Coin cells may have Alkaline chemistries, with a cell voltage of 1.5V. This drops to 0.9V when discharged. 

Applications that require higher voltages may use Li-ion coin cell batteries, which are also widely available. This type of cell offers 3.0V when fully charged, dropping to 2.2V when discharged. There are many variants on the exact Li-ion chemistry used, which maximise the different properties. For example, type BR maximises the battery’s capacity – Panasonic’s best BR coin cells have capacities up to 500mAh (BR3032). Type CR, on the other hand, minimises the battery’s internal impedance, which means it can supply higher pulse currents.

Also at the periphery of the Internet of Things are some wearable accessories with similar power profiles, such as heart rate monitors that communicate data back to a sports watch or smartphone. Some wearables are able to harvest enough energy from the wearer’s movements that they can use this to power their electronics, however, energy as a power source can be unpredictable and may not coincide with the active period for the electronics. Most energy harvesting devices therefore require a rechargeable battery which is charged by the energy harvesting subsystem, so that energy can be used as and when it’s needed.

 

 

 

 

 

Rechargeable coin cells are available with excellent energy densities. For example, Varta’s Coin Power series (left) offers nominal 3.7V batteries, 5.4mm high, measuring 12.1mm (diameter) for the 50mAh capacity and 16.1mm for the 100mAh capacity version. These button cells, as small coin cells are often called, offer low internal impedance and discharge currents up to 5C (that is, 250mA or 500mA, respectively). 

Outside of coin cells, other small lightweight battery form factors for wearable devices include Panasonic’s pin type rechargeable battery (right), intended for thin applications like spectacle frames and pens. This 3.75V battery measures 3.5mm (diameter) by 20mm, and weighs just 0.6g. Rechargeable coin cells are available with excellent energy densities. For example, Varta’s Coin Power series offers nominal 3.7V batteries, 5.4mm high, measuring 12.1mm (diameter) for the 50mAh capacity and 16.1mm for the 100mAh capacity version. These button cells, as small coin cells are often called, offer low internal impedance and discharge currents up to 5C (that is, 250mA or 500mA, respectively). 

Industrial Temperatures

Aside from consumer electronics, the Internet of Things also encompasses the automotive and industrial environments. For industrial process control in particular, installing wireless sensors to tell a central system what is going on all over a factory is a big part of enabling Industry 4.0. Industrial sensor networks may use energy harvesting, perhaps from heat energy expended in the process itself, or from the movement of a robotic arm, but they still require batteries. Though the power profile may be similar to consumer devices, batteries for these applications will need to withstand much harsher environments and maintain reliability though conditions are difficult. Specialised casings and seals can prevent dust, moisture and chemical ingress, but it can be hard to protect against very hot and very cold temperatures that affect the batteries’ chemistry.

Tadiran’s battery for harsh environments

 

For harsh environments like these, Tadiran has developed AAA and AA format batteries which may be charged at temperatures between -40 and 85°C, a big improvement on typical Li-ion rechargeables which operate over the range 0 to 60°C. This type of battery is actually a hybrid layer capacitor (HLC) which can produce the current pulses needed for wireless communication, up to 5A. They also offer a low self-discharge rate, less than 5% per year, and are expected to last more than 10 years in the application. 

Ultimately, the choice of battery for any application in the Internet of Things will depend on the power profile of the application, in combination with any environmental factors such as temperature. If you need advice on battery performance, click the Ask an Expert button to the right of this post to get in touch with one of our regional technical specialists in your local language.

Want more like this? Sign up for our newsletters

About Author

Tim Parker Photo
Tim Parker

With over 20 years' experience in the electronics industry, working for Micromark and then Avnet, Ti...

Design Trends: Batteries For Iot | Avnet Abacus
Contact our product specialists

Ask an expert

Have a question? Our regional technical specialists are on hand to help.

Design Trends: Batteries For Iot | Avnet Abacus
Related Articles
A group of colleagues working in a computer security room having a discussion
Advanced solution for kiosk devices with ARM architecture
2024年11月22日
CUSTOM S.P.A. seamlessly transitioned to Windows 10 IoT Enterprise on ARM64 for multiservice kiosks
factory showing IoT data on screens above the machines
When edge and enterprise collide
By Philip Ling   -   2023年3月9日
See the building blocks of a connected world at Embedded World 2023
Design Trends: Batteries For Iot | Avnet Abacus
Related Events
2025-05-AVA-EBV-Training-and-Events-General-Spotlight-768x432
Advanced Engineering in Belgium
Date: 2025年5月21日
Location: Online, On demand
Related Designs Menu