Custom Meta Tags
Hero Banner

Pressure Sensors: The Design Engineer's Guide

Long Copy_3-AW

Pressure sensors: The design engineer's guide

The advent of smaller, lower-cost and lower-powered pressure sensors has increased efficiency and performance, and generated a new wave of innovation, in both the sensors themselves and their applications. As demand for these technologies is increasing, the worldwide pressure sensor market is estimated to grow to $11.4 billion by 2024. With a variety of different sensor technologies now available on the market, it can be difficult to know where to start.

The Design Engineer’s Guide to Pressure Sensors was created to help you understand the types of sensors in common use, their operating principles, and their modes of use (absolute, gauge, or differential). Whether you’ve designed with pressure sensors before or not, this field guide is intended to provide a comprehensive overview of the technologies, insight into the various applications, and assistance in finding the sensor that’s right for your design.

Further down this page, you’ll find an introduction to how pressure sensors work, or you can jump ahead to the most relevant chapters for you:

Pressure Sensors Contact GBL

Need some advice on pressure sensors?

Our pressure sensor experts are on hand to help you make the right choice for your application.

Pressure Sensors Chapter 1 GBL

Chapter 1

How pressure sensors work

An introduction to pressure sensors covering the different types, how they work, their function, construction, and what to consider in your design choices.

Pressure sensors chapter 1 graphic
Pressure sensors chapter 4 GBL

Chapter 4

Pressure sensor output signals

Sensors, transducers, or transmitters? The right selection is important for your application. So what's the difference and how do you choose between them?

Pressure sensor guide chapter 4 graphic
Pressure sensors chapter 7 GBL

Chapter 7

Pressure sensors for different media types

An in-depth guide to pressure sensors for different media types. Learn about the technology, applications, different options, their specifications and their limitations.

Pressure sensor guide chapter 7 graphic
Pressure Sensors Chapter 2 GBL

Chapter 2

Pressure sensor applications

Discover the recent innovations in pressure sensor technology that are enabling smarter, safer, and more environmentally friendly electronics for businesses and consumers alike.

Pressure sensor guide chapter 2 graphic
Pressure sensors chapter 5 GBL

Chapter 5

Types of pressure measurement

What’s the difference between absolute, gauge and differential pressure sensors? And how do you know which one to use?

Pressure sensors guide chapter 5 graphic
Pressure sensors chapter 8 GBL

Chapter 8

Pressure sensing in harsh environments

An in-depth guide to pressure sensors for harsh environments - designing for extreme temperatures, high pressure, and corrosive and dynamic environments.

Pressure sensor guide chapter 8 graphic
Pressure Sensors Chapter 3 GBL

Chapter 3

The different types of pressure sensors

Discover how pressure sensors vary according to the type of pressure measurement, sensing principles, output signal, media, MEMS technology, mounting and more.

Pressure sensor guide chapter 3 graphic
Pressure sensors chapter 6 GBL

Chapter 6

The core pressure sensor technologies

What’s the difference between the different pressure sensor technologies? And how do you know which one to use?

Pressure sensor guide chapter 6 graphic
Pressure sensors chapter 9 GBL

Chapter 9

Understanding specifications

Explore the datasheet and the different factors affecting the accuracy of pressure sensor readings. Discover how to make the right choice for your application.

Pressure sensor guide chapter 9 graphic
Pressure Sensor Linecard

Pressure sensor linecard

Click the image to view our pressure sensor linecard.

Right Rail Card Dark

Webinar

Discover the keys to designing pressure sensor applications with this 30-minute technical presentation and Q&A with Nicholas Argyle, Applications Engineer EMEA, TE Connectivity.

Watch On Demand
Right Rail Card Dark_1

White paper

Need a more digestible introduction to pressure sensors? Download the white paper, 'Pressure sensors: Design considerations and technology options'.

Download
Right Rail Card Dark_2

Sensor solutions brochure

Discover the latest sensor solutions available from Avnet Abacus.

Download
Right Rail Card Dark_3-RB

Sensors linecard

Explore our pan-European sensor suppliers and their products and solutions.

Learn More
Right Rail Card Dark_3-KI

New products

Discover the latest product announcements from our sensor suppliers.

Learn More
Static HTML
 

 

Pressure sensors introduction

An introduction to pressure sensors

Since there are many different types of applications for pressure sensors, there are many types of sensors available with a wide variety of characteristics, whether it’s for harsh or corrosive environments, medical equipment or mobile devices. Selecting a pressure sensor means choosing from a vast array of technologies, packages, performance levels and features in order to meet multiple demands for accurate pressure measurement, such as:

  • Gas pressure inside a tank, such as an industrial-compressor reservoir
  • Measuring level or volume of liquid contained by sensing the pressure at the bottom of a vessel
  • Measuring pressure differences between two points in a system, as a means of monitoring or quantifying the flow of liquids or gases
  • Barometric pressure: change in atmospheric pressure with weather conditions or with altitude. Useful in weather stations, environmental monitoring, or to assist navigation dead reckoning alongside GPS or cell triangulation
     

What is pressure?

Pressure = Force / Area

In SI (MKS) units, a force of one Newton, applied to an area of one square meter, exerts a pressure of one Newton per square meter, or one Pascal.

Any kind of pressure sensor contains a mechanism or structure that reacts proportionately to a force applied. The area over which the force is applied is constant, for a given sensor structure.

There are three different types of pressures that can be measured: gauge, absolute, and differential.

Gauge pressure description

Gauge pressure

Gauge pressure is the pressure measured relative to the ambient atmospheric pressure. It can be positive for pressures higher than atmospheric, or negative for lower pressures. A gauge pressure sensor will have two ports, allowing the media at the reference pressure, and at the pressure. A typical application for a gauge pressure sensor is to measure liquid levels in a vented tank using the difference in hydrostatic pressure and ambient atmospheric pressure.

You can read more on gauge pressure in chapter five: types of pressure measurement.

Cross-section of a typical gauge pressure sensor
Mixed Media_2

Absolute pressure

Absolute pressure sensors will give the result relative to zero (a perfect vacuum). Sensors will have one port for the media to enter and exert pressure on the sensing element, producing a positive change in output, of magnitude proportional to the pressure applied.

This is useful in applications that are measuring atmospheric pressure, perhaps to determine altitude. Absolute pressure sensors are also used in pressure measurement applications that will be used at different altitudes, since atmospheric pressure varies with altitude, gauge pressure wouldn’t give an accurate reading. This type of sensor is used in tyre pressure monitoring systems to optimise tyre performance. 

For more on absolute pressure sensors, head to chapter five.

Cross-section of a typical absolute pressure sensor
Mixed Media

Differential pressure

Differential pressure sensors measure the difference in pressure between two points, similar to how a gauge sensor works. But in this case the reference pressure is one of the points in the system, as determined by the system designer. The change in differential output is positive or negative, depending on which is greater. The magnitude of the change is proportional to the pressure difference between the two domains. 

As an example, differential sensors are sometimes used to detect the pressure difference either side of an object. Differential pressure sensors are often used to monitor airflow in HVAC applications.

In chapter five we explore differential pressure sensors in more detail.

Cross-section of a typical differential pressure sensor
Long Copy_1

Construction

To an extent, the operating principle – absolute, gauge or differential – determines the sensor’s construction. An absolute pressure sensor may be designed to respond to pressure applied at the top side or the back side, when mounted on a circuit board or a panel, for example. Creating a port for the measured media to enter through the top side may leave the sensor vulnerable to hazards such as physical damage or contamination with dirt or moisture. A bottom-side entry sensor may be chosen to overcome this. The diagrams below compare the layout of both types.

A diagram of top-side or bottom entry absolute pressure sensors

A gauge sensor is typically designed to allow atmospheric pressure to apply to one port, while permitting the measured pressure to be applied to the other.

Similarly, a differential sensor will feature two ports, through which each of the measured media is designed to come into contact with the sensing element. The diagram below compares the construction of gauge and differential sensors.

Examples of gauge (left) and two-port differential (right) pressure sensor packages

 

Pressure sensor, transducer, or transmitter?

It is worth noting that “pressure sensor” is a generic term to describe a pressure-sensing device that may be a sensors, a transducer or a transmitter, depending on the design of associated electrical circuitry.

The sensing element responsible for detecting and quantifying the effects of applied pressure produces an output that cannot be used directly in an electronic circuit – like a microcontroller-based system. The physical response needs to be translated into an electrical signal, and then signal conditioning is required to create a suitable, usable signal.

Mixed Media_3-AU

Pressure sensors

Pressure sensors produce an output voltage that varies with the pressure it experiences, usually referring to the sensor element that is physically detecting the pressure. Packaged board-mount pressure sensors are available which will require the designer to consider calibration, temperature compensation and amplification separately. Confusingly, the phrase “pressure sensor” is also sometimes used to describe transducers and transmitters in general.

ALPS HSPPAD042A digital pressure sensor
Mixed Media_3-ML

Pressure transducers

Pressure transducers, like pressure sensors, produce an output voltage that varies with pressure. A transducer in this context is a sensing element combined with signal conditioning circuitry, perhaps to compensate for temperature fluctuations, and most likely an amplifier to allow transmission of signals further from the source. Note that for most applications there is an advantage to specifying pressure transducers that are temperature compensated rather than trying to implement custom temperature compensation on a pressure sensing element, as the testing required can be complicated and difficult.

TE Connectivity MEAS M5600 pressure sensor
Mixed Media_3-PH

Pressure transmitters

Pressure transmitters are similar to transducers, but generate a current signal across a low-impedance load rather than a voltage signal. Typically the output will be a 4-20mA standard industrial output. Be aware that in portable applications, transmitters can wear the batteries down if they are consistently used at the top end of their pressure range. 

TE Connectivity AST44LP
Long Copy

Specifying absolute pressure sensors where they aren’t really required is a common mistake; the majority of industrial applications can use gauge pressure. It’s important to fully understand the application’s requirements before making a selection to ensure an accurate, efficient and economical choice.
 

Working principle of a pressure sensor

An electronic pressure sensor relies on a physical reaction to applied pressure, and then measuring the resulting proportional change electronically. Commonly used phenomena include changes in capacitance, or changes in ohmic resistance of a strain gauge or piezoelectric element, which are proportional to the magnitude of the deflection when pressure is applied.

Important criteria such as measurement range, environmental suitability, physical size, and power requirements, and the type of pressure measurement required will have a significant guiding influence on engineers looking for an application specific solution.

Mixed Media_3-QV

Capacitive pressure sensors

A capacitive pressure sensor contains a capacitor with one rigid plate and one flexible membrane as electrodes. The area of these electrodes being fixed, the capacitance is proportional to the distance between the electrodes. The pressure to be measured is applied to the flexible-membrane side, and the resulting deflection causes a change in capacitance that can be measured using an electrical circuit.

The diagram to the right (click to expand) illustrates the operating principle behind capacitive pressure sensing.

Cross section of a capacitive pressure transducer
A capacitive pressure transducer relies on capacitance change produced by deflection of the membrane, which alters the capacitor geometry
Strain gauge pressure sensors MM

Strain-gauge pressure sensors

In a strain-gauge type pressure sensor, foil or silicon strain gauges are arranged as a Wheatstone bridge. The strain gauge is attached to some kind of diaphragm, which deflects when pressure is applied. The resulting signal is then measured, amplified and conditioned by the Wheatstone bridge circuit to provide a suitable transducer-voltage or transmitter-current output representative of the applied pressure, as shown in the diagram to the right. 

 

 

A circuit diagram of a bridge type sensor
A circuit diagram of a bridge type sensor
Piezoresistive pressure sensors mixed media

Piezoresistive pressure sensors

Piezoresistive sensing elements can also be arranged in a similar bridge formation. The diagram below illustrates how the sensing elements of a bridge-type pressure sensor are attached to a flexible diaphragm, so that resistance changes according to the magnitude of the diaphragm deflection.  The overall linearity of the sensor is dependent on the stability of the diaphragm, over the stated measurement range, as well as the linearity of the strain gauges or piezoresistive elements.

A diagram of a piezoresistive pressure sensor operating principle
Piezoresistive pressure sensor elements measure resistance changes according to the magnitude of diaphragm reflection
Long Copy_2

MEMS sensors

It’s easy to imagine a piezoresistive or capacitive pressure sensor as a large device like a through-hole electronic component or a module ready to screw into the side of a tank – but that’s not always the case.

A piezo or capacitive pressure-sensing mechanism can also be fabricated on silicon as a MEMS (Micro Electro Mechanical System) device and packaged as a compact surface-mount device typically measuring only about 2-3mm per side.

MEMS devices, which include not only pressure sensors but also motion or position sensors, and silicon microphones, are extremely small, stable, and cost-effective, bringing advanced functionality to space- and cost-constrained equipment like mobiles and IoT endpoints.

MEMS devices are fabricated in silicon using doping and etching processes. These processes are performed at chip scale, resulting in a tiny device that can be co-packaged with signal-conditioning electronics. The electronic circuitry may comprise simple amplification to produce an analogue output, and may also include analogue-to-digital conversion to generate a digital output.

An analogue output may be advantageous if the sensor signal is to be handled entirely in the analogue domain, or if the designer wants to use an ADC of particularly high resolution or accuracy, or if the system-host microcontroller contains a suitable integrated ADC on-chip. A digital sensor can be designed-in with no need for external conversion components, thereby saving overall component count.

Perhaps the easiest type of sensor to visualise is a barometric pressure sensor. These can be used for measuring ordinary atmospheric pressure, and are used in a range of  applications including context sensing or indoor navigation in smartphones. Typically, this is a tiny MEMS sensor.

Detecting changes in atmospheric pressure enables the device to theoretically be able to calculate its height above sea level – for example on a road (to assist satellite navigation and aid dead reckoning in the event of loss of satellite signal), or to detect what level of building the user is situated, such as in a multi-storey car park, office block, apartment block, or shopping mall.
 

Design considerations

Understanding the types of sensors in common use, their operating principles, and modes of use (absolute, gauge, or differential) can help engineers make initial selection decisions when identifying the most suitable sensor to choose for a given application.

The materials used and type of construction can have an important influence over aspects such as the measurement range, limiting factors like the maximum survivable pressure to which a sensor can be exposed, its stabilising time after soldering, and long-term stability in the intended application.

An understanding of the electrical output properties, and the circuitry needed to interact properly with the host electronic system – typically a microcontroller- or microprocessor-based control system — can help assess how the choice of pressure sensor will influence the likely electronic integration challenges.

This introduction only scratches the surface of pressure sensor technology. Chapter 1.2 will explore the different types of sensing elements that are used in pressure sensors, how they work, and their advantages and disadvantages. If you're looking for more detail on anything discussed here, you can check out the later chapters of this guide below. Alternatively, if you're pressed for time, the full guide is available as a downloadable PDF here

For more information on our other sensor technologies, visit our sensors page.

Omron 2SMPB Barometric Sensors Product Spotlight

OMRON

2SMPB barometric pressure sensors

2SMPB-02B and 2SMPB-02E sensors provide stable, reliable height and pressure measurements for changes in elevation of as little as 2m, making them ideal for drones, car navigation and altitude meters.

Omron release two new Barometric Sensors for battery operated mobile devices.
TE Connectivity HTU21D and MS5637 BLE Wireless Sensor TAG Demo V1.1 - Product Spotlight

TE Connectivity

HTU21D and MS5637 BLE wireless sensor

TE Connectivity introduces the sensor tag demo V1.1 reporting humidity, temperature and barometric pressure through a standard low power 2.4GHz wireless communication protocol. Samples are available to request from Avnet Abacus now.

TDK - EPCOS C33 and C39 series MEMS pressure sensor dies Product Spotlight

TDK

C33 and C39 series MEMS pressure sensor dies

TDK introduces the new EPCOS C33 and C39 MEMS pressure sensor dies for automotive and IoT applications.

New miniaturized EPCOS sensor dies for automotive and IoT applications.
Grid Box Light

Bourns

BPS130 series MEMS pressure sensor

The BPS130 series MEMS pressure sensor features harsh media compatibility and high temperature operation with high accuracy.

Bourns BPS130 series MEMS pressure sensor
Pressure Sensors Chapter 2 GBD

Chapter 2

Pressure sensor applications

Discover the recent innovations in pressure sensor technology that are enabling smarter, safer, and more environmentally friendly electronics for businesses and consumers alike.

Pressure sensors guide chapter 2 graphic
Pressure sensors chapter 6 GBD

Chapter 6

The core pressure sensor technologies

What’s the difference between the different pressure sensor technologies? And how do you know which one to use?

Pressure sensor guide chapter 6
Pressure Sensors Chapter 3 GBD

Chapter 3

The different types of pressure sensors

Discover how pressure sensors vary according to the type of pressure measurement, sensing principles, output signal, media, MEMS technology, mounting and more.

Pressure sensor guide chapter 3 graphic
Pressure sensors chapter 7 GBD

Chapter 7

Pressure sensors for different media types

An in-depth guide to pressure sensors for different types of media. Learn about the technology, the applications, the different options, their specifications and their limitations.

Pressure sensors guide chapter 7 graphic
Pressure Sensors Chapter 4

Chapter 4

Pressure sensor output signals

Sensors, transducers, or transmitters? The right selection is important for your application. So what's the difference and how do you choose between them?

Pressure sensor guide chapter 4 graphic
Pressure sensors chapter 8 GBD

Chapter 8

Pressure sensing in harsh environments

An in-depth guide to pressure sensors for harsh environments - designing for extreme temperatures, high pressure, and corrosive and dynamic environments.

Pressure sensor guide chapter 8 graphic
Pressure Sensors Chapter 5 GBD

Chapter 5

Types of pressure measurement

What’s the difference between absolute, gauge and differential pressure sensors? And how do you know which one to use?

Pressure sensor guide chapter 5 graphic
Pressure sensors chapter 9 GBD

Chapter 9

Understanding specifications

Explore the datasheet and the different factors affecting the accuracy of pressure sensor readings. Discover how to make the right choice for your application.

Pressure sensor guide chapter 9
Long Copy_3-NP

Products and suppliers

Avnet Abacus works with some of the best suppliers of pressure sensors in the world. Our team of pan-European technical specialists work closely with them to offer you the highest level of engineering support for your designs. If you have a question on pressure sensors, or you would like some advice on sensor selection, visit the Ask an Expert page to get in touch

Supplier teaser TE (GBL)

Supplier

TE Connectivity

TE Connectivity offers a wide range of digital and analogue board level pressure sensors, media isolated pressure sensors and pressure transducers.

A range of TE Connectivity pressure sensors
Panasonic Pressure Sensors GBL

Supplier

Panasonic

Panasonic offers a wide portfolio of high precision and accuracy relative (gauge) pressure sensors. These sensors are available with or without an on-board amplifier.

Panasonic pressure sensors
Amphenol Advanced Sensors Pressure Sensors GBL

Supplier

Amphenol Advanced Sensors

Amphenol Advanced Sensors offers a range of MEMS pressure sensors including surface mount, hybrid, and media isolated types for medical, industrial and transportation applications.

A range of Amphenol Advanced Sensors pressure sensors
SMI Pressure Sensors GBL

Supplier

SMI

SMI (now part of TE Connectivity) develops and manufactures MEMS-based pressure sensors that serve challenging applications in the automotive, medical, and industrial markets.

A range of SMI pressure sensors
Omron Pressure Sensors GBL

Supplier

Omron

Omron offers several gauge and absolute pressure sensors for measuring air pressure as part of its MEMS portfolio. Omron’s devices offer small size, low power consumption and good temperature dependency.

An omron pressure sensor
TDK Pressure Sensors GBL

Supplier

TDK

TDK's lineup of pressure sensors ranges from miniature media-resistant sensor elements with extended temperature ranges to high-precision pressure transmitters with analog or digital output.

Murata pressure sensor die
Bourns Pressure Sensors GBL

Supplier

Bourns

Bourns's line of environmental sensors based on MEMS technology includes pressure sensor models ideal for a range of applications including industrial automation, energy, building and home control and medical devices.

InvenSense Pressure Sensors GBL

Supplier

TDK InvenSense

The InvenSense barometric pressure sensor family is based on MEMS capacitive technology which provides ultra-low noise at the lowest power, enabling industry leading relative accuracy, sensor throughput, and temperature stability.

InvenSense pressure sensor
NPI Product Table

New products

ImageProductNew
Retrieving Products...
Static HTML_1