FAQ Hero Banner

The Question and the Answer

MaaXBoard-Accessories
MaaXBoard-Accessories
MaaXBoard Supported Accessories
MaaXBoard  MaaXBoard Mini  MaaXBoard Nano  MaaXBoard RT  
Question:

 

What accessories are supported by Avnet out of box by the MaaXBoard portfolio?

 

 

 
Answer:

The MaaXBoard's support the following accessories, do a quick search on Avnet.com to find them.

  • AES-AXX-MAAX-PWRUL - This is a 5 volt 3 amp USB type C power supply that is compatible with all MaaXBoards.
  • AES-ACC-MAAX-DISP1 - This is a 7-in MIPI-DSI capactivite touch display that enables applications that require display capability. This display supports resolutions up to 1280*720. This diaply is only compatible with the MaaXBoard platforms.
  • AES-ACC-MAAX-CAM1 - This is a MIPI-CSI camera that features the a high quality OV5640 image sensor that is designed to be electircially compatible with Raspberry Pi or MaaXBoard platforms.
  • MCU-LINK - The MCU-LINK is a JTAG/SWD debugger in addition to a UART TTL 3.3V I/O converter. The JTAG/SWD debugger functionality is used on the MaaXBoard RT to program the hyperflash memory for application development. The UART TTL converter can be used on all MaaXBoards to communicate to the console over the 3.3V 40pin GPIO header(UART). 
  • AES-SQN-MNRCHGO-HT1-G - This Pi HAT enables LTE connectivity through the Monarch Go Modem to your Pi HAT compatible device. It supports CAT-M1 connectivity via the Verizon ThingSpace network. In addition the Monarch Go modem is is end product certified on the Verizon LTE network allowing an easy low cost transition from prototype to production.
MaaXBoard-Accessories