FAQ Hero Banner

The Question and the Answer

Minized - [Place 30-58] IO placement is infeasible
Minized - [Place 30-58] IO placement is infeasible
Minized - [Place 30-58] IO placement is infeasible
MiniZed  
Question:

I have the 2017.2 Vivado project from github, I have built this and generated a petalinux builds which boots on the minized.

My next task was to add some IP, as an initial simple test I have just changed the axi_gpio_1 to dual mode and added an output mapped to M9, I have the following set in the constraints file:

set_property PACKAGE_PIN M9 [get_ports pl_gpio_test]

set_property IOSTANDARD LVCMOS33 [get_ports pl_gpio_test]

When I generate in vivado I get the following error:

[Place 30-58] IO placement is infeasible. Number of unplaced terminals (1) is greater than number of available sites (0).

The following Groups of I/O terminals have not sufficient capacity:
IO Group: 0 with : SioStd: LVCMOS18   VCCO = 1.8 Termination: 0  TermDir:  Out  RangeId: 1 Drv: 12  has only 0 sites available on device, but needs 1 sites.

Term: pl_gpio_test_tri_o[0]

If I look at the I/O bank properties in vivado  the output is correct on bank 35, pin M9, LVCMOS33, output.

I have been using a zybo board before and have not seen this error before and there doesn't seem to be much about it on the internet.
 
Can you direct me on what to do next?

Answer:

Changed the constraints to:

set_property PACKAGE_PIN M9 [get_ports pl_gpio_test_tri_o]

set_property IOSTANDARD LVCMOS33 [get_ports pl_gpio_test_tri_o]

You have to add a _tri_o to the end of the port name in this project.

Vivado appends your signal name with "tri_i" or "tri_io" or "tri_o" depending on the IO type when the Create HDL wrapper script generates the wrapper.  The appended name depends on whether the signal is defined as input only, input/output, or output only respectively within your GPIO block.

For information on tracking down IO placement errors, see the discussion on this Xilinx thread:

https://forums.xilinx.com/t5/Implementation/IO-Standard-default-when-XDC-clearly-defines-location-and-io/td-p/781856

Minized - [Place 30-58] IO placement is infeasible