FAQ Hero Banner

The Question and the Answer

Mouse and Keyboard not responding with USB OTG
Mouse and Keyboard not responding with USB OTG
Mouse and Keyboard not responding with USB OTG
PicoZed  
Question:

I just got my PicoZed SDR and followed the directions for startup and I cannot get my mouse or keyboard to respond.

Answer:

Just to be clear, you're plugging the USB hub into the same Micro USB to USB A socket that you plugged the USB mouse into. You can't use a Micro USB to USB A cable (like a phone charger style cable) to plug the board into a hub.
 
You have to use a Micro USB OTG host dongle and then plug the USB hub into that cable, and then the USB keyboard and mouse into the hub.  If the PicoZed SDR is working fine when you plug the mouse and keyboard in directly, I'd say you either have the hub hooked up wrong, have defective hubs, or possibly need a hub that's powered externally (though the PicoZed SDR should be able to handle the current of the hub, KB, and mouse). A few different hubs have been tested without issue.

Mouse and Keyboard not responding with USB OTG