FAQ Hero Banner

The Question and the Answer

Sobel Vivado HLS Kernel using AXI Stream interface
Sobel Vivado HLS Kernel using AXI Stream interface
Sobel Vivado HLS Kernel using AXI Stream interface
ZedBoard  
Question:

Is there any example of Sobel Vivado HLS Kernel using AXI Stream interface?

Answer:

A sobel filter implementation created with HLS and integrated as a peripheral in Zynq Design using AXI 4 Stream protocol. A comparison in the performance of the peripheral opposed to the SW-only code in -O3 mode (3x  acceleration).


Project URL: 
https://fpgaw0rld.wordpress.com/2017/05/16/sobel-vivado-hls-kernel-using-axi-stream-interface/

Sobel Vivado HLS Kernel using AXI Stream interface