FAQ Hero Banner

The Question and the Answer

Testing code on QEMU
Testing code on QEMU
Testing code on QEMU
ZedBoard  
Question:

Can you write up a brief tutorial on how to get your ARM code running in QEMU to see how it runs without having to have hardware?

Answer:

This is a flow I hadn't thought of, but I do agree it is definitely a useful topic to write about.

First, if you are on Windows, you will want to get your self setup with VirtualBox to bring up a 64 bit Linux environment.

Next, get QEMU downloaded and up and running.

You also need to get your ARM development environment up and running. The alternative to this is to download and install the Xilinx tools, and then do your ARM code development in the Xilinx SDK tool. 

Ok, now we are to the point where, regardless of you being on Windows or Linux, you are good to go for configuration.

So let's write a simple hello world c program, cross compile it for ARM, push it to the qemu machine, and then run it. 

First, let's write our hello world program. I usually use vi to edit files, however here I will just use the cat command so I can show you what the file contents are:

    zynqgeek@beth:~$ cd
    zynqgeek@beth:~$ mkdir arm-devel
    zynqgeek@beth:~$ cd arm-devel/
    zynqgeek@beth:~/arm-devel$ touch helloworld.c
    zynqgeek@beth:~/arm-devel$ cat > helloworld.c
    #include
    int main()
    {
    printf("Hello World!\n");
    return 0;
    }
    ^C

Where the ^C is hitting ctrl-c on your keyboard.

Ok, now that I have my file, we need to compile it (note if this doesn't work go back and follow the instructions for setting up your development environment).

zynqgeek@beth:~$ arm-linux-gnueabi-gcc -o helloworld helloworld.c

Ok, now that we have our file, we need to get it to our qemu virtual machine. To do this, we are going to do need two command terminals open, so pop open another xterm or open another ssh session.

In terminal window 0, we are going to be running qemu - this simple will just be executing a single bash script. In terminal window 1 we will be ftp'ing our file to the qemu VM.

In terminal 0:

*navigate to where you have downloaded and uncompressed the zynq_linux.tar.gz archive*

    root@sue:~# cd zynq_linux/
    root@sue:~/zynq_linux# ./start_qemu.sh


    ...
    Starting rcS...
    ++ Mounting filesystem
    ++ Setting up mdev
    eth0: link up (1000/FULL)
    ++ Starting telnet daemon
    ++ Starting http daemon
    ++ Starting ftp daemon
    ++ Starting dropbear (ssh) daemon
    rcS Complete
    zynq>

So let's make sure that we now have our ftp server up and running on our qemu vm.  We will list the processes that are running:

    zynq> ps | grep "ftpd"
      600 root       0:00 tcpsvd 0:21 ftpd ftpd -w /
      620 root       0:00 grep ftpd
    zynq>

We see two items, the first is our ftp server - woot!  The second is the command of us looking for the ftp server.

Note:  If do not see the server running, you can execute this command:

       zynq> tcpsvd 0:21 ftpd ftpd -w /&

Cool!  Now all we need to do is go to our terminal 1 and make a connection to our qemu VM ftp server and upload our helloworld program.
If you take a look in the start_qemu script, you will see that there are a number of port forwarding assignments, specifically port 21 (the tcp/ip port that ftp uses) is forwarded to port 10021 locally.  So we will make our connection on that.

In terminal 1:

    zynqgeek@beth:~/arm-devel# ls
    helloworld  helloworld.c
    zynqgeek@beth:~/arm-devel# ftp localhost 10021
    Connected to localhost.
    220 Operation successful
    Name (localhost:tim): root
    230 Operation successful
    Remote system type is UNIX.
    Using binary mode to transfer files.
    ftp> put helloworld
    local: helloworld remote: helloworld
    200 Operation successful
    150 Ok to send data
    226 Operation successful
    7797 bytes sent in 0.00 secs (104304.9 kB/s)
    ftp> quit

Now, jump back to terminal 0 (our qemu VM):

    zynq> cd /
    zynq> ls
    README          lib             opt             sys
    bin             licenses        proc            tmp
    dev             linuxrc         ps              update_qspi.sh
    etc             lost+found      root            usr
    helloworld      mnt             sbin            var
    zynq> chmod +x helloworld
    zynq> ./helloworld
    Hello World!
    zynq>

COOL!
One quick note: Don't forget the chmod +x command - the file won't have execution privileges when being created by ftpd, you need to add those.

Conclusion

So there you have it, this is a nice way to test our your arm code without needing hardware in the loop.  Enjoy!

Note: Since the output of SDK is an .elf file, I am still working on the best way to get your code over from SDK to qemu. I do believe there is a how-to on this from Xilinx, but I can't find it right now - I will check again in the morning.

Testing code on QEMU