Article

How will Matter help us meet the smart home promise?

Walter Puhl
person holding smartphone with home in background
The opportunity for smart home growth drives Matter. In 2023 over half of the homes in developed economies were using at least one smart device.

What's Next Magazine

The smart home has been hyped in the media since the term was first coined by The American Association of Home Builders in 1984. But the idea goes back to 1975 and the introduction of the X10 communications protocol, which was designed for data communications over AC power lines in buildings.

Since then, many wired and wireless networking protocols have emerged to meet the needs of various applications in this sector. Examples used in building automation include KNX, an open standard based on the European Installation Bus (EIB) communication stack. Low energy applications benefit from EnOcean, whose unique selling point is running from harvested energy such as the kinetic energy generated by pressing a light switch.

The digitally addressable lighting interface standard, DALI, is used almost exclusively in industrial and commercial lighting control systems. Zigbee and Z-Wave are competing encrypted protocols developed for smart homes and other buildings and the first to really leverage mesh networking. Industry alliances were formed to promote all these standards and ensure interoperability within their respective ecosystems, but not interoperability between them.

In 2015, the Thread consortium was formed. Its goal was to create an IPv6-based wireless protocol for delivering secure, robust, reliable and easy-to-use networks. Being IP-based, Thread devices can connect directly to IP-enabled hubs, routers, smartphones, tablets and other devices. Thread simplifies network design by removing the need for central hubs or bridges.

Matter takes this concept further. The Connectivity Standards Alliance (CSA, formerly the Zigbee Alliance), positions Matter as "The Foundation for Connected Things" and describes it as an IP-based protocol to connect compatible smart home devices and systems, mobile apps and cloud services.

The Matter project started in late 2019 and the first edition of the standard was published on October 4, 2022. Version 1.2 was released a little over a year later, on October 23, 2023, expanding support for more home devices.

The smart home is still an emerging market

The opportunity for smart home growth drives Matter. The demand was created in 1975 but it wasn’t until 2023 – nearly half a century later – that analysts concurred that over half the homes in developed economies were using at least one smart device.

But that could mean just one smart speaker, a connected thermostat, or networked utility meter per home. A single smart device hardly demonstrates that the smart home dream has come true. Unacceptable complexity for users and lack of interoperability have been cited as the two main barriers to delivering smarter homes. Matter looks to address these issues and drive the smart home market to greater maturity.

More about Matter

The logic behind Matter is simple: it’s an application layer protocol that works on any IPv6 network and provides support for Ethernet, Wi-Fi and Thread mesh networking. This is important because products and services from different vendors using Matter will now communicate seamlessly, eliminating many proprietary hubs and protocol translation requirements.

The Matter project is a collaborative effort lead by the CSA (Connectivity Standards Alliance) between Amazon, Apple, Samsung SmartThings and leading semiconductor manufacturers. These companies see Matter as a way of accelerating the growth of the smart home market by making device development easier, giving consumers a greater choice of compatible smart home products and services, and making home networks easier to understand and use.

From door locks to fridges and robot vacuum cleaners to security cameras, using Matter should mean consumers only need one app and controller to manage and monitor all the smart devices in their homes, instead of one per ecosystem. There is now at least one Matter-compatible smart EV charger available, as part of a home energy management system.

Support for Wi-Fi and Ethernet is particularly significant because most smart home protocols were designed for devices that operate at low data rates. Smart utility meters are a good example. However, high-definition video from cameras demands high bandwidth connectivity and Matter is the first protocol suited to both types of data.

Many homes already have one or more Matter controllers, even if they’re not labeled as such. For example, most hubs, displays and smart speakers from Amazon, Apple, Google and Samsung running the latest software versions include this functionality. Matter is also built into Android and iOS operating systems, which means smartphones and tablets can be used to control Matter-enabled home network devices.

block diagram

Semiconductor companies are embracing Matter

From the outset, semiconductor companies saw the opportunity that Matter offers. The project now enjoys the support of around 200 firms. Almost every smart home device is based on a microcontroller (MCU) or a system-on-chip (SoC), and Matter source code tree is freely available on GitHub. Avnet Silica’s engineers help make it easy for its semiconductor supplier partners to support Matter-enabled product design.

Many homes will have smart devices that have been added over time and consumers will be reluctant to ditch existing products. To that end, software development kits support bridging between Matter-enabled and non-Matter-enabled devices, eliminating another potential barrier to adoption. Of course, developers will need to write the code to integrate the Matter API into their solution and handle data transfers from the home system to the Matter API. Once done, everything in the smart home environment can be controlled using just one platform, irrespective of the ecosystem or manufacturer.

How much progress has the Matter protocol made?

Every new protocol has limitations and imperfections, at least at the outset. In less than two years, Matter has made remarkable progress as an enabling technology for smart homes. It could be argued that this technology has done more for the smart home than any other development since X10 in 1975. It's the breadth of devices supported by Matter and the subsequent transformation of the customer experience that validate this as a breakthrough.

At the Embedded World show in Nuremberg in April 2024, Avnet Silica demonstrated how solutions from H&D Wireless, Nordic Semiconductor, NXP, Panasonic Industry, STMicroelectronics and U-blox can work together, thanks to Matter’s interoperability across platforms and devices.

An Apple HomePod, Google Nest Hub and Amazon Echo were shown running Matter over Thread to control a range of devices. These included a Panasonic board based on a Nordic Semiconductor chipset, and NXP and ST boards, all with Bluetooth connectivity. A Nordic Semiconductor weather station that transmitted its data to other devices using Matter over Wi-Fi was also shown.

The demonstration emphasized IoT security, which is inherent in using Matter over Thread. This highlighted the future-proof nature of the open-source philosophy that underpins Matter.

According to data aggregator Statista, the smart home market will be worth $154.4 billion in 2024, rising at a compound annual growth rate of 10.67% to hit $231.6 billion by 2028. Household penetration of the technology will rise from 18.9% to 33.2% over that period, the firm says. There seems little doubt that Matter will be instrumental in making these predictions come true.

About Author

Walter Puhl
Walter Puhl, Wireless technology specialist

Walter Puhl is a wireless technology specialist, working for Avnet Silica across EMEA. His experienc...

Helpful Links

Marketing Content Spots
Related Articles
Related Articles
tst
A supply chain professional's guide to thriving in uncertainty
By Robert Cowan   -   July 15, 2025
Today's professionals must master the art of strategic patience while building systems robust enough to weather whatever storm comes next. The winners will be those who respond most intelligently and avoid a knee-jerk reaction.
Outdoor installation of huppe basketball hoop can weather the elements.
AI-powered huupe dreams come true
By Valeri Oliver   -   April 21, 2025
See how Avnet helped usher in a new era of basketball technology. Think of it as the Peloton of basketball, an innovative basketball hoop using AI and computer vision components.
Related Events
Related Events

No related events found

how-will-matter-help-us-meet-the-smart-home-promise