Article

Know your bonds: LOCA, OCA & Air Gap

graphic of person
person in a clean room

Today, touch displays are a familiar sight in industrial applications, so making sure that they are robust and durable, while also maintaining their brilliance, is essential. This means that we pay particular attention to how each component of the display is connected – a process called ‘optical bonding’. 

There are three kinds of transparent optical bonding used to connect the display, touch sensor and cover glass:

  • Full Surface Bonding (which uses UV-cured liquid adhesive, known as LOCA – Liquid Optical Clear Adhesive)
  • Adhesive Film (called ‘OCA’ or ‘Optical Clear Adhesive’)
  • Air Gap Bonding

Learning LOCA

With this technique, the air gap between the display and touch sensor/cover glass is completely sealed using liquid adhesive. This is achieved using a dosing system which precision dispenses the adhesive according to the geometry of the display. With this technique, the touch sensor or cover glass can be applied without a single bubble. No bubbles equal no annoying reflections (because there are none between each surface), and at the same time the color brilliance and contrast are increased.

infographic of touchscreen, LOCA, LCD

But, for industrial or outdoor applications, the layer of LOCA also intensifies impact resistance and prevents particles or moisture coming into contact with any components, which could cause permanent damage or, at the very least, compromise the image quality.

OCA, on the other hand, seals the air gap with adhesive film, which is, once again, applied with precision and then bonded to the touch sensor or cover glass. It’s a swifter process, as there is no wait for the adhesive to cure, and there is little to no thermal stress to the components. This technique too has the benefit of creating a robust, impact resistant display. Both LOCA and OCA also significantly minimize splintering of the display if it meets with a destructive force. 

However, there are some less positive aspects of LOCA to consider. During the curing process, it’s possible that some areas are outside of the reach of the UV, and this can lead to air bubbles – sometimes even delamination. Because of the nature of the bonding, as soon as any contaminants or bubbles appear, the entire screen has to be replaced. For an already complex and costly process, this can be very problematic.

Air Gap Bonding

Here, we use a high-performance double-sided adhesive tape frame, which connects the display and touch unit with an air gap remaining between them, hence the name. This type of bonding is probably the easiest and simplest way to connect a display unit, which reflects in the cost. It’s a particularly strong and stable bonding technique, overall, as well as being highly versatile. It can be used to bond low-energy surfaces (such as PE and PP) or many other plastics and powder coatings.

infographic of air gap bonding

Unlike LOCA/OCA bonding, it doesn’t have the advantages of increased readability, minimization of reflection and protection against dust and dirt particles. It also creates a comparatively thick structure, but this can be adjusted by selecting different tape sizes. There can also be issues around reduced adhesion due to an uneven surface in the cover glass. Plus, the introduction of any dirt or grease can cause components to detach.

Ultimately, it’s important to understand that there is no hierarchy when it comes to bonding – no technique is ‘better’ or ‘worse’ than the other. They simply have different qualities which are context appropriate. So, it’s always a good idea to understand the pros and cons of each process to ensure that you’re selecting the best option for your display.

infographic showing optical bonding vs no optical bonding

infographic showing optical bonding vs no optical bonding

infographic showing optical bonding vs no optical bonding

Of course, our display experts are on hand to guide you in your choice of bonding and the creation of your display or touch solutions. Find out how Avnet Displays can propel your product innovation and get in touch today.

Contact a Display Solutions Expert

About Author

graphic of person
Alexander Sommerfeld, Solution Manager Display Integration, Avnet Displays

After getting his diploma in mechatronics, Alexander entered the world of display solutions at MSC i...

Additional Information

Avnet’s Displays team solves product design challenges for OEMs looking to build the perfect display technology into their products. Our in-house team works directly with businesses to solve all the challenges of integrating a display into a product design, from tiny wearables to massive outdoor screens. We design, build and deliver display solutions all over the world for established household brand names and industry disruptors alike.  If you need a display designed and integrated into your product, our team is here to help. Get in touch today to tell us about your challenge.

 

Marketing Content Spots
Related Articles
Related Articles
flower on a screen
Transparently brilliant: the new Simple Plus Open Frame
By Stefano Rosato   -   April 3, 2025
Adaptable to any aesthetic or location, and ready for anything, our stunning new transparent OLED monitor, ‘Simple Plus Open Frame’, is so incredibly crystal clear, we can hardly take our eyes off it.
A row of digital signage on a pathway at night, with a person jogging in the distance.
Stylish, powerful and ready for anything – our latest outdoor displays
By Stefano Rosato   -   February 10, 2025
Our new IP-Rated outdoor displays are so stylish, durable and energy efficient, they can actually improve the look of the spaces they’re in.
Related Events
Related Events

No related events found

know-your-bonds-loca-oca-and-air-gap