Article

Over-the-air broadcasting returns with perks

NextGen TV
How well will NextGen TV fare against the constantly changing array of streaming services?

For most people, over-the-air (OTA) broadcast TV is either a distant memory or the stuff of old-timey TV watching lore.

As households increasingly replace cable with streaming services, can OTA TV broadcast still compete?

Many say yes. The reasons? Today’s OTA broadcasts, called NextGen TV, offer a combination of benefits no other content delivery option can: interactivity with greatly enhanced picture clarity and audio quality.

In the beginning

The story of NextGen TV begins at least four decades ago when the federal government, the National Association of Broadcasters (NAB), and private industry envisioned that OTA TV transmission architectures would transition from analog to digital. After many years of haggling over specifications, regulations, and other details, digital TV broadcasting came into focus as did efforts to bring it to fruition.

It’s difficult to overstate the challenges faced by the broadcasting, content, and TV manufacturing industries when transitioning from analog to digital transmission. It was a massive undertaking that included spectrum auctions, channel reallocations, development of new transmission blueprints, aspect ratio conversion, expensive equipment changes, and more. As of 2009, legacy tuners could no longer receive OTA broadcasts in the U.S. so the most onerous of these tasks was to modify tens of millions of televisions to accept digital OTA signals.

Although stations broadcasted in both analog and digital forms for several years, consumers needed to update their TVs with adapters at their own cost.

With this in mind, the government provided up to two $40 coupons for digital-to-analog converters for each household. Like rapid COVID-19 tests today, demand exceeded expectations and allocations fell short. Still, most everyone who needed the converter got one.

This and other factors resulted in three postponements of the analog-to-digital conversion deadline that only in June 2021 appears to have ended. The last holdout was Alaska, granted an extension because of the state’s unique combination of small remote populations and extreme weather that made deployment extremely difficult.

Fortunately, the previous hard work makes the transition to NextGen TV much easier for consumers, thanks in large measure to advances in semiconductor, RF, and digital signal processing technologies that reduce the size and cost of the required converter.

For retrofitting existing TVs, the solution is a small box connected to the TV’s RF coaxial input. Most major TV manufacturers have already integrated the tuner within their latest models, and all will have them in the next few years. This leaves the antenna, but as NextGen TV signals are far more robust than their predecessors, these antennas no longer need to be massive roof-mounted structures of years past. Today, they are small enough to fit behind the television, on or near windows, and in rare cases outdoors.

So, what do you get?

Within its 20 sub-standards and 1,000 pages of specifications, Advanced Television Systems Committee (ATSC) 3.0 defines what advantages consumers can expect from NextGen TV, and they’re impressive.

Although it operates at the same frequencies as existing channels and access remains free, the true benefits lie in NextGen TV’s hybrid architecture. Signals captured over the air combined with the broadband connection to the internet make it interactive. NextGen TV combines the two-way communication capabilities and other features available only via an IP-based connection.

NextGen TV supports legacy SD video resolution up to 720 x 480, interlaced HD video resolution up to 1920 x 1080, progressive-scan 4K UHD video with resolution up to 3840 x 2160, and frame rates up to 120 fps. To achieve its spectral efficiency, NextGen TV uses H.265 HEVC (High-Efficiency Video Coding) rather than MPEG-2 used in ATSC 1.0. So, while the channel width remains 6 MHz wide, it can transmit more video channels at higher resolution in half the bandwidth.

ATSC 3.0 also has better audio compression via Dolby AC-4 for 5.1 to provide excellent sound quality and up to seven audio channels. The standard also integrates video enhancement features such as High Dynamic Range (HDR), High Frame Rate (HFR), and Wide Color Gamut (WCG). It also supports mobile reception so viewers can access live local and national news, sports, and entertainment on mobile devices without relying on cellular networks.

Public safety is one of the most important beneficiaries of the new standard. It expands the current minimal capability provided by the Emergency Alert System (EAS) to a new Advanced Warning and Response Network (AWARN). For viewers, this means that in addition to the usual text and tone alerts, it can deliver photos, surveillance video, storm tracks, evacuation routes, shelter instructions, hospital wait times, power outage locations, and other information. AWARN also “wakes up” devices that are not powered on.

Monetizing the technology

A big benefit for broadcasters and their advertisers is the ability to collect personal information they can use to micro-target advertising to individual users based on their viewing and buying habits and other metrics.

By merging OTA antenna TV with the internet, local stations will be able to personalize news, sports, live events, and shows with interactive features. Broadcasters never had this ability before as there was no two-way path between the station and the user.

Now, when a user watches an ad, they can use a remote control to click on a link that brings them a webpage and enables the user to perform all activities now associated with web browsers or smartphone apps.

With all the competition and promotion from streaming, cable, fiber to the home, and increasingly fixed wireless access at millimeter-wave frequencies, NextGen TV has received much less exposure.

The big question is how well it will fare against the constantly changing array of streaming services that increasingly provide access to local stations as part of their bundles. As the deployment of NextGen TV expands throughout the country, it won’t be long before we get an answer.

Marketing Content Spots
Related Articles
Related Articles
you-are-here-token-on-a-map-inside-a-shopping-mall
Bluetooth 6.0 vs. Bluetooth 5.4: Key advantages
By Avnet Staff   -   October 24, 2024
Bluetooth 6.0 comes with six new features of note. With centimeter-level positioning one of them and now available, will this change the way we navigate?
Satellies orbiting Earth
What happens when non-terrestrial and cellular converge?
By Carolyn O'Connor   -   August 5, 2024
OEMs and start-ups are paying attention to a development that places cellular and satellite technologies on a path to convergence. The growth of connected devices and associated traffic blurs the line between satellite and terrestrial networks.
Related Events
Related Events
satellite in orbit
Space 2.0: AMD Technologies for New Space
Date: February 23, 2022
Location: Webinar
over-the-air-broadcasting-returns-with-perks