Article

What to consider when choosing a connector (interconnect solution)

Jamie Peterson
engineer assembling connectors

What are you connecting?

What is being connected, both electrically and physically.  Are you connecting a high current power source, a high-speed data line or a low voltage sensor output?  All three of these will have different requirements and bring differing considerations to the design process.

And let’s not forget the physical aspect.  You may have a limitation on board space or height based on your product.  As technology advances, more features and capabilities are being designed in and products are getting smaller.  This puts a spotlight on miniaturization and products like the Molex Pico-EZmate Slim connectors which have a mated height of 1.20mm.

Where are you connecting?

Is the connection going to be in an enclosure sitting in a climate-controlled environment like an office or will it be in a harsh environment?  And that begs the question, what type of harsh environment?  Types of harsh environments can range from temperature - extreme heat or cold; harsh chemicals - gasoline or solvents; Liquid - oceanic equipment that’s exposed to salt water; force -mechanical stress or vibration; radiation such as cosmic rays.

Each harsh environment relies on a specific type of material in the connector’s construction to combat the environment and maintain the integrity of the signal. The connector’s housing not only needs to insulate each pin or plug from one another, but also helps determine its use case(s) – resistance to oil or solvents, stability in heat and cold or withstands water.

An example of a harsh environment connector is the Molex FPC-to-board Connector for EV Battery Management.  These products are anti-vibration and anti-dust/condensation.

The material and size of the contacts are equally important.  For a high-power application, a larger Bus bar is necessary.  In a high-speed application, gold contacts prevent data loss.  Gold plated connectors work best in RF applications due to the “skinning effect” where most of the signal travels on the outer “skin” of the conductor.

How many connections do you have?

This is also referred to as circuit density, or the number of circuits a connector can accommodate per square inch.  A high-density connector eliminates the need for more connectors, saving space in tight engine compartments.  The Molex high-density flexible-printed circuit (FPC) cables not only pack a high number of connections into a small space but are also flexible for space-limited applications.

Wire Gauge

The gauge of wire required in the application needs to be considered as well and ties into the current rating.  Heavier wire gauge is needed in higher current situations or when mechanical strength is required in the wire.  Most connectors cover common automotive wire gauges of 16 to 22 AWG.

Are you approved?

Ensuring that your design’s connectors have been tested to the same specifications that your project requires will lead to an easier final approval process.  Most connectors are UL (Underwriters Limited) approved.  Further approvals may be required by Society of Automotive Engineers (SAE), Canadian Standards Association (CSA) or Ingress Protection (IP).

Making solid, safe connections is essential to keeping your signals, power and end users secure. Avnet has experts to help you find the products to meet your design needs and speed up. the connector selection process. 

About Author

Jamie Peterson
Jamie Pederson, Technical Content Manager

Jamie Pederson is a Technical Content Manager with Avnet. He has 18 years of electronics industry ex...

Marketing Content Spots
Related Content
Molex campaign, electric vehicle dashboard
 
 
Increased demand for ADAS and autonomous driving are pushing automakers to add more electronic control units and next-gen domain control units to vehicles resulting in a need for reliable interconnect solutions in harsh environments.
 
Related Articles
Related Articles
Vibe coding using AI on a computer screen
Will vibe coding kill the compiler?
By Philip Ling   -   2025年7月3日
There is an ever-growing number of high-level programming languages to choose from. With vibe coding using AI assistants becoming popular, could the days of high-level languages, toolchains and even compilers be numbered?
development board and tablet with balloons on screen
Big, bright, built for engineers: New Display Kits for ST Discovery Boards
By Frank Ploenissen   -   2025年6月30日
Size does matter. At least it does when it comes to our new MIPI DSI displays. We’re upscaling your options with new 7” and 10.1” display kits, designed to fit seamlessly with STMicroelectronics’ STM32F769I and STM32H747I Discovery kits.
Related Events
Related Events
airplane cockpit looking out on the runway
More Electrification in Aircraft
Date: 2022年10月11日
Location: Virtual
what-to-consider-when-choosing-a-connector