From development tools and components to design help, testing and production supplies, prototyping can be a time-consuming process. Not to mention considerations around testing, assembly and regional compliance. Luckily, our resources can help guide you.
Interconnect technology is designed for nearly every application imaginable including medical products. Molex designs and develops cutting-edge standard products with the quality and reliability that meet the rigorous needs of the medical industry.
SiC will soon overtake Si as the dominant semiconductor material for power devices with voltage rating higher than 600V. Designers looking to stay competitive and lower long-term system costs are turning to SiC-based technologies good reason.
The promises of lower energy costs, increased productivity and greater reliability, and the pressures from emissions regulation, are driving rapid EV innovation in agricultural and other off-road equipment.
Through rapid prototyping, Amphenol developed sensor modules that reliably detect carbon dioxide and hydrogen from cell decomposition venting for early warning of lithium cell thermal runaway.
Are you tempted to take an engineering shortcut in your next design? Take one supplier partner engineer’s experience and advice that there’s an excellent chance it will come back and bite you.
The sand is shifting between what is real and what is virtual. If the result is the same, does it matter? The engineering community is embracing virtual prototyping to increase innovation and reduce time to market.
We live in the age of over-the-air updates and constant upgrades. These can be used to fix bugs, but they are also used to deliver value-added or paid-for features. Does that make the concept of prototyping redundant?
For RF engineers working on mmWave applications, limited access to hardware and test equipment can mean delays, cost and complexity. Remote testing over a secure internet connection lets engineers jump directly to application development.
Edico Genome’s DRAGEN Platform is changing the way clinicians diagnose and treat deadly diseases like cancer by giving them crucial genetic information at unprecedented speed, scale and accuracy.