You’ve accomplished this by an improved ability to sense, analyze and deliver treatment via state-of-the-art medical equipment and by empowering individuals to take a more active role in their personal health. Ready to be a part of the next wave of innovation? Avnet has been there every step of the way and continues to be your key partner in making breakthrough applications come to life.
Avnet serves the distinct needs of customers in each of these four major healthcare segments:
- Diagnostic and therapeutic equipment
- Medical imaging systems
- Medical instrumentation
- Fitness and healthcare wearables

Accelerating the innovation process
Just like you, we think in terms of an overall system. To help you create your next-generation solution, we’ve designed highly integrated development tools, including a wide range of sensors that provide you with better access to underlying data, processors optimized for specific functions such as running algorithms for image processing; and critical-support areas including connectivity, input/output (I/O) and power management.
Dedicated experts focused on the healthcare industry
No one understands the complexities and challenges around the healthcare industry better than you. We recognize this and field a staff of technical and operations professionals whose sole focus is supporting this segment.
Our team comes from a medical OEM background. They stay current on the latest sensing, processing and embedded computing technologies, as well as, emerging regulatory requirements and overall market trends.
Avnet is an authorized source for the leading suppliers of technologies revolutionizing the medical industry. Our technical and business development teams have direct access to the medical business units at these suppliers. We’ve fostered these relationships through the insights and knowledge we demonstrate. That means when you work with our team, you get market insight ahead of the curve.
ISO certified value-add and integration centers at your service
Outsourcing with the right partner is a strategic way for you to keep your costs down without sacrificing quality or control. Freeing up cash from operations means more dollars for R&D, delivering new services or impacting the bottom line. Avnet holds the ISO 13485:2003 certification at all of our integration centers around the world. Our processes ensure consistent quality to your exact specifications, including when you make changes to your BOM or application.
Avnet has been consistently recognized as supplier of the year by the leading brands in the medical industry for well over a decade. We know what it takes to serve the medical industry and invite you to put us to work for you.

The right mix of products in stock is the prescription for success
We understand that some medical applications take years to reach the market. We also know that for emerging breakthrough applications such as wearables, it’s all about fast time to market. With Avnet you get the benefit of a partner able to support both.
We stock products that are on seven to ten year long life programs so you don’t have to worry about design changes at the end of a long test and approval process. We also have tailored supply-chain programs to make products available for you well after end-of-life announcements to support your equipment in the field or spare parts programs.
When time to market is critical, our inventory is in place to support you. We intentionally invest in stocking the newest releases, such as highly-integrated sensors, so you can hit your market windows with cutting edge solutions.
Ready to see how our knowledge, access, and expertise can speed processes and reduce costs throughout your business? Contact your local Avnet medical expert to learn more or complete this form and we’ll connect with you shortly.

New Product
AUBoard 15P FPGA Development Kit
The AUBoard 15P provides the flexibility and versatility for engineers to experiment with and learn the AMD Artix UltraScale+ ™️ architecture. Target applications include Embedded Vision, wired communications, and industrial networking.

Avnet XRF8 Xilinx RFSoC Gen3 System-On-Module
Designed for integration into deployed RF systems demanding small footprint, low power and real-time processing, featuring the Xilinx Zynq®️ UltraScale+™ RFSoC Gen 3 ZU47DR, with 8 RF-ADC, 8 RF-DAC channels and 6 GHz RF bandwidth.

ZUBoard 1CG
Flexible and versatile.Great for designing complex experiments for Artificial Intelligence and Machine Learning, and for investigating the AMD-Xilinx Zynq® UltraScale+™ architecture, Vivado and Vitis!

New Product
MaaXBoard OSM93
MaaXBoard OMS93 features the NXP i.MX93 processor to enable EdgeLock® secured, accelerated AI applications using an on-board NPU. Target applications include edge AI, industrial automation, smart appliances, EV chargers, fleet management.

RZBoard V2L
A vision-AI accelerated development board in popular single board computer format with well supported expansion interfaces. Ideal for development of cost-efficient Vision-AI and a range of energy-efficient Edge AI applications.

Technical Articles
Monitoring impact levels in sports
Concussion, also known as mild traumatic brain injury (MTBI), is a very serious topic in the world of sports today.