Site Guidelines
Components
3 Panel Spotlight V1
Overview
The three panel spotlight v1 component has three small graphics/icons, a title and a little bit of content. The graphic and the title will act as the CTA in the panels.
Images
Image sizes should approximately be 432 x 432.
Title
The 3 panel slide up has an overall optional title for the component.
Overview (component body text)
This is a basic blurb about the overall context of the component.
Panels
Each of the three panels have their own title, body text and CTA
Component fields
Enter the overall title for the component here. This field is optional.
Enter the body text for the component here. This field is optional.
Enter your panel title here. This field is required.
Enter your body text here. This field is required.
Enter your CTA info here. This field is required.
Click Select to add the image. The library selection will pop up. Go to the Global Asset Library and click through to your image location. Select it and click OK. Don't forget to provide alt text for the image. These fields are required.