Custom Meta Tags
Hero Banner

Components

Component Documentation

Hero Banner

Image

The size for the hero image is 2000 X 240

**Please ensure the image is optimized for the web. File must not be larger than 100KB

Hero Title

1. The title for a hero banner should be title case - upper case on the first letter of each major word

2. You have two options for the title color: Black or White

3. The hero title is limited to 45 characters maximum

Component elements

Please note all elements with an asterisk next to the element title are required.

Example:

Click Select to add/modify the image. The library selection will pop up. Go to the Global Asset Library and click through to your image location. Select it and click OK.

Add your title here. Please note the title is limited to 45 characters maximum.

Click the drop down to select the title color. Options are White (default) or Black.

Save and Close your changes.

Related Components