AMD develops highly flexible and adaptive processing platforms that enable rapid innovation across a variety of technologies – from the endpoint to the edge to the cloud. AMD is the inventor of the FPGA, hardware programmable SoCs and the ACAP, designed to deliver the most dynamic processor technology in the industry and enable the adaptable, intelligent and connected world of the future. For more information, visit www.amd.com.


AMD Smart Door Lock
Step into the future of home security with smart door locks, where cutting-edge technology meets convenience. One standout innovation in door locks is the integration of camera-based AI systems for face-recognition.

Motor Control Solutions
Digital motor control can be defined as a drive system that combines an electric motor with power electronics for its energy delivery and processor units for motion control, as well as sensor and communication interfaces.

AMD Kria™ Adaptive Motor Control SOMs
AMD is focused on developing power-efficient and highly deterministic industrial solutions suitable for large-scale deployments. The AMD Kria™ starter kit offer a latency advantage when compared to competitive products.

AMD Kria™ SOM Family
AMD Kria™ SOM Family is ideal for Edge and Vision Application Development and features a custom custom-built Zynq™ UltraScale+™ MPSoC device in a small form factor card.

Adaptive & Intelligent Healthcare Solutions from AMD
Technological advancements that are creating solutions for earlier detection, better imaging, and virtual and robotic-assisted care have the ability to help healthcare providers increase patient outcomes and provide more effective personalized care.
AMD ZUBoard 1CG
The ZUBoard 1CG provides the flexibility and versatility for engineers to experiment with and learn the AMD Zynq™ UltraScale+™ architecture.


AMD Industrial Robotics
Discover how the AMD Kria™ robotics starter kit, along with the Kria™ robotics stack, enables rapid development for robotics, machine vision, and industrial communication and control, through adaptive computing.
AMD Kria™ KR260 Robotics Starter Kit
The AMD Kria™ KR260 Robotics Starter Kit integrates high-performance industrial interfaces and features native ROS 2 support. It enables roboticists and industrial developers without FPGA expertise to develop hardware accelerated applications.


Driving Automotive Innovation with AMD
From automation to electrification to infotainment and beyond, we’re helping our customers like you deliver the next generation of cutting edge automotive designs.

AMD MiniZed Development Board
Featuring a AMD Zynq™ Z7007S, which integrates an Arm Cortex-A9 processor with AMD Artix™ 7 programmable logic, the MiniZed is a low-cost yet versatile development board targeted for entry-level Zynq designs.
U250 Alveo™ Data Center Accelerator Cards
Learn about Xilinx® U250 Alveo™ Data Center accelerator cards, designed to meet the constantly changing needs of the modern Data Center.

Webinar: Getting Started with the Ultra96-V2 Development Board
This training is held by Mario Bergeron. Mario is a Technical Marketing Engineer for Avnet, specialized in embedded vision and machine learning. After his degree in Computer Engineering (B.Sc.) from Université Laval in Québec City, he started his career as an ASIC designer, and has since then accumulated over 25 years of DSP and FPGA based embedded design experience. Present activities include deep learning platforms, reference designs, and customer training.

Accelerating AI Camera Development with AMD Vitis™ Software Platform
Check out the On-Demand webinar from AMD. During this webinar we will explore this topic from a variety of different perspectives.

AMD: Cost-Optimized Portfolio for Industrial Cameras
This presentation explores some of the trends driving new processor requirements in industrial cameras and provides examples of Xilinx's recent solutions that offer increased performance per watt and unlock intelligence, resolution, and speed for compact form factor cameras