High-power solutions for fast EV charging from Infineon
The combination of rising number of electric vehicles on the market and pressure from governments to reduce vehicle emissions to zero by 2050 at the latest, are the main reasons why, there is a great need for more efficient charging solutions. As various consumer studies show, the acceptance of electromobility depends to a large extent on the availability and duration of the charging process. High-performance DC charging stations are the answer to these market requirements. Already today, a typical electric vehicle can charge about 80% of its battery capacity in less than 10 minutes. This is comparable to refueling a conventional car with an internal combustion engine.
As the market leader in power electronics, Infineon supports you in realizing energy-efficient DC charging concepts. Benefit from one of the most comprehensive product and design portfolios on the market, covering the full range of power conversion, microcontrollers, safety, auxiliary power supply and communications.
Fast DC EV charging - whitepaper
Realizing the future of fast EV charging through CoolSiC™
Charging the electric vehicle while grabbing a coffee sounds like a myth? As the EV market is set to grow exponentially, massive investment plans in new vehicle models and infrastructure are pushed by government initiatives.
Especially during long journeys limited charging infrastructure can hinder the move to private electric vehicles. With SiC power semiconductor devices for fast DC chargers delivering 350 kW, a charging time of less than ten minutes becomes feasible.
Whitepaper content:
- Charging options
- Selecting an optimum charger topology
- The inherent advantages of SiC MOSFETs in DC chargers
- Speeding up the design of EV DC chargers
- Adding EVs to the sustainable energy mix
- Fast charger challenges beyond improving power density
download now
Podcast4Engineers: Fast EV Charging
Today, a DC charger with 150 kW can put a 200 km charge on an EV in around just 15 minutes. As fast charging and battery technologies continue to evolve and improve in the near future, experts anticipate the charging time to drop even further. Listen to our Podcast4Engineers episodes as our Infineon experts discuss the latest trends and challenges in EV charging and how our one-stop product and design portfolio can help design energy-efficient DC EV chargers today.
listen hereInfineon Technologies EasyDUAL™ CoolSiC™ MOSFET
Our new EasyDUAL™ CoolSiC™ MOSFET modules in a half-bridge configuration were updated with a new aluminum (AlN) ceramic. This advanced material will support customers in high power density applications like Solar, UPS, traction auxiliary inverters, or even ESS and EV Charger.
Learn MoreInfineon Technologies IMZ120R030M1H
The CoolSiC™ 1200 V, 30 mΩ SiC MOSFET in TO247-4 package build on a state-of-the-art trench semiconductor process optimized to combine performance with reliability. In comparison to traditional silicon (Si) based switches like IGBTs and MOSFETs, the SiC MOSFET offers a series of advantages.
Learn MoreInfineon Technologies IMW65R048M1H
CoolSiC™ MOSFET technology leverages the strong physical characteristics of silicon carbide, adding unique features that increase the device performance, robustness, and ease of use. The IMW65R048M1H CoolSiC™ MOSFET 650V is built on a state-of-the-art trench semiconductor, optimized to allow no compromises in getting both the lowest losses in the application and the highest reliability in operation.
Learn MoreInfineon Technologies IMZA65R027M1H
CoolSiC™ MOSFET technology leverages the strong physical characteristics of silicon carbide, adding unique features that increase the device’s performance, robustness, and ease of use. The IMZA65R027M1H CoolSiC™ MOSFET 650V is built on a state-of-the-art trench semiconductor, optimized to allow no compromises in getting both the lowest losses in the application and the highest reliability in operation.
Learn More
EV Charging: The Power of Three
Discover how to shorten your time-to-market with end-to-end EV charging infrastructure solutions from EBV, Avnet Abacus and Avnet Embedded.
EBV Design Hub
Browse and review hundreds of proven reference designs to accelerate your design process. Our designs can be modified and saved in our AVAIL design tool and then exported to your CAD tool of choice.

Ready to take the next step with your EV charging designs?
Discuss your requirements in detail with our EV charging experts.