Nexperia Custom Meta Tags
Manufacturer Hero Banner

Franchised Partner

nexperia-title

Nexperia

nexperia-bio-body

Nexperia is a dedicated global leader in Discretes, Logic and MOSFETs devices. This new company became independent at the beginning of 2017. Focused on efficiency, Nexperia produces consistently reliable semiconductor components at high volume: 85 billion annually. The company’s extensive portfolio meets the stringent standards set by the Automotive industry. And industry-leading small packages, produced in their own manufacturing facilities, combine power and thermal efficiency with best-in-class quality levels. Built on over half a century of expertise, Nexperia has 11,000 employees across Asia, Europe and the U.S. supporting customers globally.

Manufacturers Categories Static HTML
Nexperia Featured product highlights (LC)

Featured product highlights

EBV - Product Highlights - Nexperia GaN FETs (GBL)

Nexperia GaN FETs

Nexperia e-mode GaN FETs are ideal for low-power 650 V applications or high-power 150 V applications. Nexperia cascode GaN FETs are the enabler in industry 4.0 and renewable energy applications offering high power density, high and performance.

EBV - Product Highlights - Nexperia IGBTs in 600V (GBL)

Nexperia's IGBTs in 600V

With growing demand for robust, efficient and cost-effective power solutions across an increasing range of applications, Nexperia’s carrier stored trench-gate advanced field-stop (FS) IGBT portfolio meets these industry demands.

EBV - Product Highlights - Nexperia Silicon Carbide (SiC) MOSFETs (GBL)

Nexperia Silicon Carbide (SiC) MOSFETs

Nexperia’s new industry leading 1200 V silicon carbide (SiC) MOSFETs in D2PAK-7 surface mount device (SMD) packaging, with a choice of 30, 40, 60, and 80 mΩ RDSon values.

EBV - Nexperia Power Rectifiers Product Highlights (GBL)

Nexperia's Power Rectifiers

The range of Nexperia power rectifiers offers industry-leading solutions for various applications. They provide a wide selection, including planar Schottky, trench Schottky, SiGe rectifiers, and ultra & hyperfast recovery rectifiers.

EBV - Nexperia Load switch Grid Box Light (GBL)

Nexperia Load Switch

The NPS4053 switch limits the output current to a constant current by using a constant-current mode when the output load exceeds the current limit threshold or shorted.

EBV - Motor Control - Product Highlights (GBL)

Motor Control Solutions

Digital motor control can be defined as a drive system that combines an electric motor with power electronics for its energy delivery and processor units for motion control, as well as sensor and communication interfaces.

EBV - Product Highlights - Factory Automation Highlights (GBL)

Factory Automation

The increasingly comprehensive automation in the industry is driven by macro trends such as reshoring, i.e. the relocation of manufacturing facilities from emerging countries back to industrialised states, a global shortage of skilled labour.

EBV - Analog and Power Highlights Grid Box Light (GBL)

Analog & Power Management

The era of digitalisation is ever advancing, almost as if our world were solely represented and controlled by ones and zeros. Every physical variable – be it an audio signal, temperature, voltage – is an analog value.

EBV - Nexperia - Related Events Static HTML

Related events

Nexperia: Package Transition in Power Diodes | EBV Elektronik

EBV & Nexperia | Package Transition in Power Diodes

Online, On Demand

Join us in this webinar and get an insight into Nexperia’s power diode portfolio with a focus on efficient switching performance.

NPI Product Table
Image Product Description Link New
Long Copy

Videos

See more Nexperia videos on YouTube

Static HTML_1

 

Static HTML_2 Video2

Static HTML_3-NR Video 3

Static HTML_3-MI Video 4

EBV - Nexperia - NPI Title Static HTML