Custom Meta Tags
EBV - Markets - Hero_Banner_Animation_Living_infrastructure Static HTML
EBV - City and Infrastructure - NEW Sub Navigation
EBV - Markets - CI - Smart grid and Smart metering Main Title

Smart grid & Smart metering

EBV - Markets - CI - Smart grid and Smart metering

Making electrical distribution more intelligent is one of the primary objectives that must be achieved if society is to become truly sustainable. Through the implementation of smart grid networks, utility companies are becoming much better able to balance the supply capacity against the expectations of their client base. These networks call for more sophisticated connectivity than was employed in the distribution infrastructure of the past. This predominantly relies on bi-directional power line communication (PLC), which provides a robust and cost-effective medium for data transfer, though cellular communication is also gaining a lot of traction here. The upshot is that responsive, decentralised and adaptable electricity distribution networks can be benefitted from.

EBV - City and Infrastructure - Smart Grid and Smart Metering Static HTML

 

Through smart metering, households and commercial enterprises are now becoming much better at gauging their gas, electricity, and water usage. By accessing real-time data, they are able to look at what changes can be made to the consumption behaviour to lower their utility bills and reduce the size of their carbon footprint.

Berg Insights predicts that the number of smart meters across the European continent being used to monitor electricity consumption will be close to 230 million by 2026. Global Market Insights estimates the European smart water meter market will experience a compound annual growth rate of almost 30% in the coming years, reaching a total annual worth of Euro 2.75 billion by 2027. There are numerous different LPWAN wireless protocols that can be used to connect the meter with the display unit that the user will refer to. Among the most popular are LoRa and Zigbee. There is also Wireless M-Bus and Wired M-Bus, which have been created specifically for this purpose, both being defined by the European EN 13757-4 standard. As well as wireless technology, MCUs with strong power/performance characteristics, non-volatile memories, signal conditioning devices and display drivers are all needed.

Through non-intrusive load monitoring (NILM) algorithms, it is now possible to get detailed information on electricity consumers’ behaviour, such as what appliances they are using and when. This will be of significant value when it comes to accurately forecast the demands that the grid will be subjected to, although it is vitally important that there is still adherence to GDPR personal privacy laws.

In the past, electricity grids were dependent on a small number of large-scale generation sites such as coal fired power stations. This sort of arrangement is no longer applicable though, as the number of generation sites is increasing, with renewable generation operations of differing sizes, from commercial solar and wind plants through to microgeneration and residential sites all contributing. As a consequence of energy coming from so many distinct places, decentralised grid architectures will be mandated, with intelligence at all the endpoints where energy is being generated or stored.

The system solutions employed will need to take into account the utility landscapes of different geographic regions. Some countries may only have a few utility companies and rely on one predominant source, while others will have many utility companies and a mix of energy sources.

 

EBV - City - EV Charging - Power of 3 (MM)

EV Charging: The power of three

Discover how to shorten your time-to-market with end-to-end EV charging infrastructure solutions from EBV, Avnet Abacus and Avnet Embedded.

get started
City and Infrastructure Contact EBV (GBL)

Let's talk

Better connected through LinkedIn

Get directly in touch with our City & Infrastructure Director Andrej Orel

Design Hub landscape banner Markets Static HTML

 

Design hub landscape banner EBV

 

EBVchips Teaser Box (GBL) grey

Solutions

EBVchips

Semiconductor solutions developed with and for customers

The Quintessence (GBL) grey

Magazine

The Quintessence

Discover TQ - the free knowledge magazine from EBV

Podcast Spotlight Box (GBL) grey

Resources

EBV Podcast

Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.

Digital Event Hub Spotlight Grid Box Light (GBL)

Resources

Digital Event Hub

See all our on demand webinars and check out our upcoming events.