Conduction
During conduction, heat is transferred through the vibration of molecules in a substance. As something gets warmer, it begins to increase the vibration and movement of the molecules that it consists of. In solids, particles are closely packed together and are in direct contact. Since they are close to each other, particles that vibrate near the point of contact will pass on the vibrations to other particles nearby. The vibrations then spread throughout the object. Conduction works similarly with liquids and gases, but since the density of the particles is less, there will be less efficient energy transfer between the molecules. Conduction occurs when two things at different temperatures touch each other and energy directly transfers from the material in the hotter item to the material in the colder item at the point of contact.