Custom Meta Tags
Hero Banner

參考解決方案

Long Copy

USB type-C an ecosystem approaching perfection

Solution 2 - BODY NUMBER HERE

Universal Serial Bus (USB) is undoubtedly the greatest interface ever invented. We only need to look around us to see its success as an innovation. Connecting everything from our computer peripherals to our mobile devices, it has become a technology we cannot do without. 

The reasons for its rapid adoption is equally apparent. USB is easy to use, allows fast transmission, carries an independent power supply, and is a highly flexible connection that also hot swappable. Its advantages are unprecedented. 

As a result of its popularity, a variety of connectors have emerged to allow connection with the fast growing number of devices, namely Type-A, Type-B, Mini-A, Mini-B, Micro-A and Micro-B. This has given rise to unexpected issues. For one, the different connectors mean different cables are required. Transmission rates—which have advanced up to 10Gbps in the USB 3.1 standard—are also connector dependent. There is also the issue of limited power supply as USB is now the primary means of charging our many power-hungry devices. On a lesser note, the irreversible nature of the connectors means they have to be plugged the right way to function. A design that proves to be frustrating many a times. 

Solution 3 - BODY NUMBER HERE

One new interface is born - USB Type C

With the introduction of USB Type-C by USB Implementers Forum (USB-IF), the issues we faced have become things of the past.

This newest generation of USB is easily identifiable by its small connector which features vertical symmetry for reversible insertion. But frustration-free connection is just the tip of the iceberg when it comes to advantages. Transmission speed and power capabilities have been dramatically improved, putting unmatched functionalities in the hands of both engineers and users. 

  • Size: 8.3mm x 2.5mm
  • Direction: reversible 
  • Data transfer rate: up to 10 Gbps
  • Power supply capacity: up to 100W (5/12/20V)
  • Backward compatibility: USB 2.0 LS/FS/HS 

Table_3-TZ

 

Base Specifications

  • USB 3.1
  • July 2013
  • USB 3.1 added 10Gbps (Gen 2) support
  • USB Power Delivery
  •  Revision 2.0, Version 1.2,
      March 2016
      Revision 3.0, Version 1.0a,
      March 2016
  • USB Type-C driving   Revision 2.0 adoption   Revision 3.0 adds some emerging use features
  • USB Type-C
  • Revision 1.2, March 2016
  • Adoption continues on record track
  • USB Type-C Authentication
  • Revision 1.0, March 2016
  • New–targeted use for cryptographically   authenticating certified chargers and devices
  • USB Type-C Port Controller Interface
  •  Revision 1.0, Version 1.1,   July 2016
  • Updated–defines USB PD inter-block interface
  • USB Type-C Bridging
  • Revision 1.0, March 2016
  • New–supporting USB Type-C Authentication   applications
  • USB PD Firmware Update
  • Revision 1.0, September 2016
  •  New–enabling firmware updating of products over   USB PD
  • Audio
  • Revision 3.0, September 2016
  • Revision 3.0, September 2016
  • USB Display Class
  • In work–expected in early 2017
  • In work–expected in early 2017

 

Supported by all major OS USB Type-C is highly compatible with the dominant operating systems in the market

  • MS
  • Windows 10,   Windows Mobile
  • Windows 8.1
  • USB 3.1, USB Type-C, alternate modes, billboard, power delivery,   audio accessory and USB Dual Role support
  • USB Type-C and billboard support in an update
  • Apple
  • OS X Yosemite
  • USB 3.1, USB Type-C, alternate modes and power delivery
  • Google
  • Chrome OS
  • Android   Marshmallow
  • Supports USB 3.1 and USB Type-C, supports Alternate Modes,   Power Delivery, and USB Dual Role support
  • USB 3.1 and USB Type-C
Table_1
Application Line Card Part Number
  • Docking Station
  • TI
  • TPS65982
  • 1 To 3 Dongle
  • Fresco
  • FL7102
  • Power Bank
  • Rohm
  • BM92T1X, BD99955
  • Power PD
  • Rohm
  • STM
  • Microchip
  • Renesas
  • TI
  • BM92T1X
  • STMF052
  • UTC2000
  • R9A02G011
  • TPS25740
  • Dongle (C To DP, VGA, HDMI)
  • Fresco Logic
  • Silicon Lab
  • FL7102
  • EFM8UB1, EFM8BB3
  • Cable E-marker
  • Fresco
  • FL7001
  • Cable Redriver
  • Intersil
  • ISL35111, ISl36111
  • Audio (Headset)
  • Nuvoton
  • Dialog
  • Nuc123, NAU88L25
  • Da14195, DA7217