Custom Meta Tags
Hero Banner
Space 2 articles (SN)
Main title (LC)

8 Things to Know About AMD’s Versal Adaptive SoCs and Their Role in Space 2.0

Introduction (MM)

As satellite technology evolves and the demands of space exploration intensify, traditional processing architectures are no longer enough. The new era, often referred to as Space 2.0, calls for smarter, faster, and more resilient computing systems. At the heart of this transformation is AMD’s Versal Adaptive SoC platform. These reconfigurable devices are redefining what's possible in orbit, enabling real-time decision-making, advanced telemetry analysis, and scalable AI-driven applications. Whether you’re designing the next generation of Earth observation satellites or building autonomous deep-space systems, here are eight key things you need to know about how Versal is powering the future of space.

1. What distinguishes Versal Adaptive SoCs from conventional SoCs in terms of architecture and functionality?

Hubble telescope orbiting earth
Main body (LC)

Versal Adaptive SoCs go beyond fixed-function processors by integrating adaptive hardware, AI engines, and a network-on-chip for dynamic workloads. Unlike traditional SoCs, they can reconfigure processing resources in real time, enabling them to tackle evolving mission demands. This flexibility makes them ideal for space applications where adaptability and real-time processing are mission-critical.

2. How are the reconfigurable features of Versal Adaptive SoCs being leveraged in aerospace missions?

In space missions, these reconfigurable capabilities implement advanced processing pipelines for onboard image classification, dynamic beamforming, compression, and encryption without requiring a complete hardware redesign. Designers can repurpose the same hardware to perform new functions as mission requirements change, making them highly future-proof.

3. What role do the AI and DSP capabilities of Versal Adaptive SoCs play in spacecraft telemetry and anomaly detection?

Versal SoCs utilise onboard AI, specifically long short-term memory (LSTM) neural networks, to analyse telemetry data in real time. This enables the system to predict sensor values and flag anomalies instantly, rather than waiting for data to be sent to Earth. Their adaptive intelligent engines also handle digital signal processing tasks critical to satellite communication, Earth observation, and electronic warfare.

4. How is the robustness of Versal Adaptive SoCs against space radiation achieved through their design and manufacturing processes?

Versal devices undergo rigorous radiation testing, including exposure to protons and heavy ions. They incorporate single-event effect mitigation, built-in configuration memory scrubbing, and are fabricated using ruggedised organic flip-chip packaging. These measures collectively protect against bit flips, functional interrupts, and long-term degradation in harsh environments.

5. Considering the harsh environment of space, what design considerations extend the operational life of Versal Adaptive SoCs in long-duration missions?

Versal SoCs are engineered for longevity through thermal and mechanical resilience, advanced radiation tolerance, and efficient heat dissipation. The Versal AI Core VC1902, for instance, is qualified to support long lifetime missions, extending the viability of spacecraft operating in deep space or geosynchronous orbit.

AMD Versal (GBL)

AMD

The AMD Versal range offers high-performance CPUs, GPUs, and accelerators, integrating advanced technologies for diverse workloads in AI, HPC, and data analytics, promising efficient and scalable solutions.

AMD Logo
Conclusion (LC)

6. What technical measures are implemented in Versal Adaptive SoCs to ensure power efficiency for space-bound systems?

Power efficiency is achieved through finely tuned AI engines, low-power adaptive compute units, and collaboration with power solution providers like Renesas. Support for high-efficiency multiphase power delivery and intelligent voltage regulation ensures that SoCs like the VE2302 can meet demanding current requirements (up to 20A) while maintaining tight voltage tolerances and minimal thermal output.

7. In terms of system integration, what technical advantages do Versal Adaptive SoCs offer for aerospace system designers?

These SoCs streamline integration through embedded ARM Cortex applications and real-time processors, high-speed transceivers, and hardened IP blocks like memory controllers and DMA engines. Their network-on-chip architecture simplifies data routing within the device, reducing latency and resource contention, key factors for system-level performance in satellite applications.

8. Looking at the technical evolution of Versal Adaptive SoCs, what advancements are anticipated to enhance their aerospace applications further?

Future enhancements include greater AI engine density, further reductions in power consumption, and expanded support for quantum-resistant security protocols. Enhanced packaging for devices like the VC1902 may also considerably extend mission lifespans with Class Y qualifications, pushing the boundaries of what’s possible in space computing.

Conclusion

From high-performance AI capabilities to unmatched resilience in harsh space environments, AMD’s Versal Adaptive SoCs are engineered for the challenges of modern aerospace missions. Their flexibility, power efficiency, and system integration advantages make them a foundational technology for real-time processing and autonomy in space. As missions grow more complex and operate farther from Earth, solutions like Versal will be essential to enabling smarter, more self-sufficient spacecraft. Ready to dive deeper? Explore how AMD and its partners are pushing the boundaries of space technology in the full webinar below.

Webinar (MM)

Webinar: The future of onboard AI and adaptive processing in space applications

Watch the webinar: Versal and Space 2.0 — On revolutionising onboard processing and AI in space applications.

Join us as we hear the latest news from AMD on how their Versal adaptive SoCs provide an ideal platform for advanced signal processing in space-flight applications. Combining scalar and vector processing resources with traditional FPGA logic gates, memory, and DSP resources, these SoCs empower the integration of dense signal processing systems in challenging environments.

WATCH ON DEMAND
Working on a space project and author (LC)

Working on a Space 2.0 project?

Our experts bring insights that extend beyond the datasheet, availability and price. The combined experience contained within our network covers thousands of projects across different customers, markets, regions and technologies. We will pull together the right team from our collective expertise to focus on your application, providing valuable ideas and recommendations to improve your product and accelerate its journey from the initial concept out into the world.

WE'D LOVE TO HEAR FROM YOU!

About Author

 

Paul Leys
Paul Leys

Paul Leys is the Market Segment Manager for the Aerospace and Commercial Avionics business at Avnet Silica. He supports the Avnet Silica EMEAI A+D business with a team of local Account Managers and FAEs. He has supported this business for over 25 years and has a particular passion for the space industry. The Avnet Silica goal is to be able to offer a wide range of reliable and leading-edge electronic component solutions to its space customers. Paul holds a BSc in Electronics and Electrical Engineering from Edinburgh University.

Space 2.0 Overview (GBL)

Aerospace & Aviation

Space 2.0 Overview

We use our vast knowledge and long experience of supporting traditional radiation-hardened components to come up with innovative, lower cost, reliable radiation tolerant components. We're ready to support your next Space 2.0 project.

Earth's radiation - space 2.0 components need to be radiation hardened