Advanced Processing in Light and Heavy Vehicles
NXP Semiconductors, with a history spanning nearly five decades, has pioneered the processor market, specialising in processing solutions for vehicles. These solutions encompass a wide range of applications, including engine control, CAN, LIN, radar, and functional safety. In an era of autonomous and electric software-defined vehicles (SDVs), connectivity plays a pivotal role in facilitating the collection of real-time vehicle data for cloud services. This data, harnessed with the power of AI and machine learning, paves the way for vehicles that continuously evolve, becoming safer, more secure, and more efficient while enhancing the overall driving experience.
Challenges of Transitioning to SDVs
SDVs have become the prime focus for original equipment manufacturers (OEMs). However, transitioning from the conventional domain-based platform to full zonal platforms is a formidable challenge, as illustrated in Figure 1. Some OEMs are opting to bypass the hybrid stage, moving directly to full zonal platforms, which necessitates a complete restructuring of the vehicle’s architecture. The adoption of zonal technology offers several benefits, including enhanced security, centralised over-the-air firmware updates, reduced memory overhead, and improved integration, resulting in fewer electronic control units (ECUs) and faster response times. NXP’s contributions to this transition are worth exploring.
NXP’s extensive involvement in automotive processing has positioned it as a key player in the ongoing transformation, collaborating closely with OEMs and Tier 1 suppliers. Drawing from its experience in developing braking systems, NXP has gained valuable insights into the demands of these critical applications.
![Transition to full zonal platforms](/wcm/connect/c77ac330-eb01-4a93-9541-1dccfd548ebd/Full-zonal-platforms.png?MOD=AJPERES&CACHEID=ROOTWORKSPACE-c77ac330-eb01-4a93-9541-1dccfd548ebd-oOhrhju)
Figure 1: Evolution toward full zonal platforms: the foundation for the software-defined vehicle (Image source: NXP)
The company’s background in infrastructure communication has endowed it with the expertise to lead in vehicle network processing. Furthermore, NXP’s dedicated team specializing in biometric security for passports and banking is actively working on advanced security solutions, addressing vulnerabilities in connected systems and fostering a security-centric culture across the organisation.
Introducing the NXP S32 automotive platform
The S32 automotive platform provides scalable solutions that are designed to address current and future connectivity, security and safety challenges. For example, the S32G family of vehicle network processors provides high-performance, safe and secure processing for service-oriented gateways, domain controllers, zonal processors, vehicle computers and safety processors.
Other areas that are addressed by the S32 automotive platform are different levels of driver replacement. Integrating data from radar and vision systems, or sensor fusion, and processing it with a common software framework to up to ASIL D levels of functional safety and, supported by artificial intelligence, enable self-driving technologies. Let’s explore further how the S32 platform can help OEMs minimise the number of ECUs they use and reduce the associated costs.
Combining ECUs for all Architectures
In electric vehicles (EVs), multiple ECUs are commonly found, each serving specific functions, such as power conversion, onboard charging, traction inversion, and battery management. These ECUs, as depicted in Figure 2, each incorporate a microcontroller unit (MCU).
![The NXP S32K3 offers a scalable solution for all architectures](/wcm/connect/b0d314b5-38ae-419c-9537-5188c5a079fc/NXP-S32K3.png?MOD=AJPERES&CACHEID=ROOTWORKSPACE-b0d314b5-38ae-419c-9537-5188c5a079fc-oOhsyJO)
Figure 2: The NXP S32K3 offers a scalable solution for all architectures (Image source: NXP)
To reduce the number of required ECUs, the next logical step is the transformation of the vehicle architecture into a domain topology, which distinguishes power conversion and drive and energy management domains. This reorganisation leads to a significant reduction in the number of MCUs and associated hardware by approximately 60%.
An even more integrated approach involves the creation of a full zonal design, consolidating all functionalities into a single ECU. Achieving this integration is facilitated by transitioning within the same family of MCUs, simplifying maintenance and updates. The use of the S32 platform further eases the design process, particularly when functional safety and security are essential.
Examining NXP’s MCU offerings, we find the S32K family, representing the lower end of processing power. These microcontrollers range from 120 kbytes of flash memory, operating on an ARM Cortex-M0+ core at 48V, primarily targeting small CAN/LIN nodes. As we ascend the processing power hierarchy, multiple sub-families offer products with up to 8MB of flash memory, housing several ARM Cortex-M cores, some in lockstep configuration and others decoupled, achieving clock speeds of up to 320MHz. Some of these products also feature additional cores, such as DSP for predictive maintenance or filtering and programmable CPU cores with advanced timer capabilities, catering to the requirements of traction inverters.
On the opposite end of the spectrum within the S32 platform, the S32G3 family commands high processing power. Devices in this family boast more than 20 programmable cores, capable of handling substantial data traffic. These cores can seamlessly incorporate CAN communication with Ethernet, minimising CPU interactions. This functionality supports AI accelerators, packet forwarding engines, and low-latency communication engines, necessitating the provision of an extensive library of ready-made software by NXP.
Extending the Platform Approach to Light Vehicles
The concept of the platform approach is not limited to heavy vehicles but is also explored in the context of light vehicles, including the two-wheeler market, which encompasses e-bikes, e-scooters, and e-superbikes, Figure 2. While the aim is to reduce development costs and the number of ECUs by concentrating on similar features, the two-wheeler market presents distinct requirements. A rule of thumb is that if a driving license is necessary for a two-wheeler, OEMs and Tier 1 suppliers must adhere to the motorcycle safety integrity level (MSIL), analogous to the automotive ASIL.
Initially, functional safety for two-wheelers was excluded from the scope of the ISO 26262 standard introduced in 2011, primarily due to the unique challenges and characteristics of two-wheeled vehicles. These challenges include the criticality, severity, and controllability of ensuring functional safety, particularly in scenarios where critical components, such as the anti-lock braking system (ABS), malfunction - the degree of harm to both the vehicle and the rider is greater than in the case of a car.
![The two-wheeler market spans from e-bikes and e-scooters to e-superbikes](/wcm/connect/3d1812d7-52db-47bc-a758-c9050e88b670/two-wheeler-market.png?MOD=AJPERES&CACHEID=ROOTWORKSPACE-3d1812d7-52db-47bc-a758-c9050e88b670-oOhsKin)
Figure 3: The two-wheeler market spans from e-bikes and e-scooters to e-superbikes (Image source: NXP)
However, the growing need for functional safety, driven by safety concerns, prompted the inclusion of motorbikes within the scope of ISO 26262 in 2018.
Although lower-end e-scooters and e-bikes may not require formal functional safety procedures, their inclusion is advisable due to incidents of thermal runaway in lithium-ion batteries during home charging. While there are similarities to ASIL functional safety, two-wheelers place a greater emphasis on rider behaviour as a means of risk mitigation rather than relying on the system hardware and software. For instance, if the rider chooses to drive during heavy rain, snowfall, or icy conditions, they accept a higher risk.
Ready-made development platforms
![NXP’s S32 automotive processing development platforms](/wcm/connect/78572918-2549-42db-9b95-82fe6c23adf6/NXP-S32-processing.png?MOD=AJPERES&CACHEID=ROOTWORKSPACE-78572918-2549-42db-9b95-82fe6c23adf6-oOhrAQM)
Figure 4: NXP’s S32 automotive processing development platforms (Image source: NXP)
NXP recognises the importance of expediting system development and testing. To facilitate this, the company offers ready-made S32 automotive processing development platforms, such as the GreenBox, GoldBox, and BlueBox, depicted in Figure 4, as well as the newly introduced OrangeBox. These platforms are housed in rugged cases, suitable for direct integration within vehicles, and come equipped with a wealth of software resources. We will delve further into the OrangeBox platform.
Unified Connectivity
Modern vehicles have evolved into highly sophisticated edge devices, capable of seamless communication with the cloud and their surroundings. This connectivity enables advanced safety features, secure car access, enhanced infotainment capabilities, and more. However, this growing reliance on a multitude of wireless technologies, including vehicle-to-everything (V2X), ultra-wideband (UWB), Bluetooth, Wi-Fi, 5G, and others, has led to disjointed architecture within vehicles, potentially exposing complex cybersecurity vulnerabilities.
To address this challenge, NXP introduced the OrangeBox development platform, which consolidates all external wireless connectivity into a single connectivity domain controller. This approach simplifies hardware and software complexity, accelerates time-to-market, and enforces consistent state-of-the-art security for all wireless data entering or leaving the vehicle.
The OrangeBox platform integrates cutting-edge wireless technologies from NXP, including V2X, Wi-Fi and Bluetooth, secure car access based on Bluetooth Low Energy (BLE) and UWB, as well as analogue or digital broadcast radio. It also provides support for 4G LTE or 5G connectivity and a global navigation satellite system (GNSS) for precise location services.
At its core, the OrangeBox platform features the NXP i.MX 8XLite application processor and EdgeLock-certified discrete secure element devices, ensuring secure, unified wireless access throughout the entire vehicle. The modular design of the OrangeBox platform empowers OEMs and Tier 1 suppliers to integrate only the necessary components based on vehicle requirements and regional constraints. This adaptability is crucial as vehicles become more interconnected and complex, offering a streamlined solution to developers.
Conclusion
In summary, NXP Semiconductors has played a pivotal role in advancing processing solutions for vehicles, both in light and heavy segments. Their expertise, rooted in decades of experience, has allowed them to navigate the transition to software-defined vehicles seamlessly. By offering scalable platforms, streamlined processing, and ready-made development solutions, NXP continues to drive innovation in the automotive industry, ensuring safer, more efficient, and highly connected vehicles for the future.