Avnet Silica pioneers secure device management with a commitment to simplicity, scalability, and heightened control.
As an aggregator of cutting-edge security tools and services from our trusted suppliers, Avnet Silica demystifies the complexity of safeguarding devices. Many organizations today grapple with the challenge of self-managing security, often unaware of potential vulnerabilities.
A key facet of our strategy lies in facilitating seamless device connectivity. Recognizing that security begins with pre-configuration, we empower our customers to ready their products for connection with ease. This not only ensures a state-of-the-art security posture but also instills confidence that goes beyond mere compliance.
Romain Tesniere explains Avnet Silica's Secure Device Management and Provisioning services
Navigating Pitfalls, Optimizing Solutions
The risk of ending up with devices requiring costly rework is a tangible concern for our customers. Avnet Silica steps in as a strategic partner, helping organizations decipher the optimal solution tailored to their unique use cases. While many clients have experience with security and the development stage, scaling these measures poses a distinctive challenge. Problems often manifest when devices are already in the field, making retroactive upgrades to production and programming a formidable task.
Scalability: Our Core Strength
Avnet Silica excels in providing scalable solutions, bridging the divide between the broad range of tools offered by suppliers and our customers’ need for a scalable security solution. Our strength lies in addressing challenges before they materialize, ensuring that security scales seamlessly with growing demands. As an aggregator, we possess unparalleled expertise in all supplier solutions, positioning us uniquely to deliver the most effective customer solutions.
Welcome to a realm where security isn't just a measure; it's a mindset.
Article Series
The IoT Security Series
Read our series of IoT security articles, put together by our in-house IoT, Connectivity and Wireless experts. Find articles and resources on device provisioning, network architecture, device authentication, lifecycle management and much more.

Provisioning at Avnet Silica (Logistic Centre)
Avnet Silica has its very own warehouse and logistic centre, located in Poing, Munich. The Avnet Logistics facility is certified according to DIN EN ISO 9001, DIN EN IEC 61340-5-1 & 2 and ISO 14001 and meets high-quality standards of the automotive, naval, aviation, aerospace, telecommunications, military and medical equipment industries.
Handling device management and provisioning within our facility gives you full control of what and how the provisioning is done, offers great security options and gives you a one-stop-shop for all of your needs.

Pros | Cons | |
---|---|---|
✔ Full control of what and how the provisioning is completed | ✔ Locks the device in transportation |
✘ Requires customisation content to be ready when shipping components |
✔ Locks the device, then EMS' only need to load FW | ✔ One-stop-shop for components and services | |
✔ Avnet Silica has its own personalisation machine in our Poing (Germany) warehouse | ✔ We can handle Firmware programming | |
✔ We can handle key and certification injection | ✔ Connect to any PKI vendor (EL2GO, KeyFactor, Wisekey, Digicert...) | |
✔ Connected to SFI (STMicroelectronics) and DLM Server (Renesas) | ✔ Price per piece model |
Provisioning at EMS/OEM Production Line
Handling device management and provisioning on the testing and production line also offers more flexibility when it comes to supply chain but electronics manufacturing services must agree to 3rd party use of their machines.
Avnet Silica can provide customers with an HSM to get connected to their testing/production line and get the right certificates/keys for the right products.

Pros | Cons | |
---|---|---|
✔ More flexibility when it comes to supply chain | ✔ Control of production unit count |
✘ EMS' must agree to 3rd party use of their machines |
✔ Avnet Silica can provide customers with an HSM to get connected to their testing/production line and get the right certificates/keys for the right products | ✔ Connect to any PKI vendor (EL2GO, KeyFactor, Wisekey, Digicert...) |
✘ May need to connect your (or EMS') equipment to the internet |
✔ Connected to SFI (ST) and DLM Server (Renesas) | ✔ License business model |
Provisioning in the Field
Handling device management and provisioning in the field gives you more flexibility from both a personalisation and supply chain perspective but requires strong connectivity availability at all times and means products leave manufacturing without credentials.
Services from KeyFactor, WISeKey and NXP (EdgeLock2GO) can all be offered when you choose to handle device management and provisioning in the field.

Pros | Cons | |
---|---|---|
✔ Full flexibility when it comes to supply chain | ✔ Allows for late personalisation |
✘ Requires strong connectivity availability |
✔ When powered up, the device connects with the infrastructure to get its credentials (keys/certificates) | ✔ KeyFactor: Service offered on any type of device |
✘ Products leave manufacturing without credentials |
✔ WISeKey: Service offered on any type of device | ✔ EdgeLock2GO: Service offered by NXP |
Providing OEM-ODM-EMS' with a fully integrated secure provisioning solution
Avnet Silica partners with Trusted Objects to provide OEM-ODM-EMS' with a fully integrated secure provisioning solution, adding to any existing programming equipment or test bench, secure provisioning and secure programming capabilities.
The product, called “tops plug&go” is based on a secure box connected to the programmer which ensures a full and secure control of the production with the following features:
- Protect all sensitive data (application firmware, secrets) during the transit and during manufacturing operations, up to the programmable component
- Generate and store securely in production, keys and certificates with the secure box’s HSM (Hardware Security Module)
- Enable secure keys and certificates injection in the component and secure provisioning of the application server
- Interface with factory PKI or external PKI
- Compatible with most microcontrollers and most programming equipment or test bench
“tops plug&go” benefits
- Automate and secure provisioning at OEM-ODM-EMS factory
- Management of a proprietary PKI
- Simplify certificates and keys generation at production site
- Add value to IoT devices with a unique and strong “factory identity” per product
- Matter-compliant security at factory: device initial certificate (DAC) secure generation and secure injection in MCU or electronic board
- Protect software IP and credentials against illegal copies and cloning
- Control the right number of provisioned devices with a trusted batch report
- Deployed rapidly in any factory (full support from Trusted objects at the setup)
How tops Plug & Go fits into the device provisioning process
Image | Product | New |
---|---|---|
![]() | NXP EdgeLock® A30 Secure Authenticator The EdgeLock A30 is a ready-to-use, Common Criteria EAL 6+ certified secure authenticator that includes advanced security mechanisms, including AVA_VAN.5, with symmetric and asymmetric crypto. It has an I²C target for easy connection to MCUs/MPUs and | |
![]() | Microchip WILCS02 The WILCS02 Wi-Fi Link Controller SD Board makes it easy to connect to the cloud using a host MPU running Linux®. This SD board features the WILCS02PE, an IEEE® 802.11 b/g/n (2.4 GHz) IoT link controller module. The WILCS02 SD Board offers: A good | |
![]() | Microchip WINCS02 The WINCS02 Add-on Board is an efficient low-cost development platform to evaluate and demonstrate the features, capabilities and interfaces of Microchip's Wi-Fi4 (single band) network controller module, WINCS02PC. This add-on board is compliant to t | |
![]() | Microchip RNWF02 The RNWF02 Add-on Board is an efficient low-cost development platform to evaluate and demonstrate the features, capabilities and interfaces of Microchip's Wi-Fi4 (2.4 GHz) module, RNWF02PC. This add-on board is compliant to the mikroBUS standard and | |
![]() | NXP RW612 The RW612 is a highly integrated, low-power tri-radio wireless MCU with an integrated MCU and Wi-Fi® 6 + Bluetooth® Low Energy (LE) 5.4 / 802.15.4 radios designed for a broad array of applications, including connected smart home devices, enterprise a | |
![]() | STMicroelectronics MPUs STM32MP13 lines STM32MP13 microprocessor series from single Arm® Cortex®-A7 up to dual Arm® Cortex®-A7 and Cortex®-M4 cores runs from 650 MHz up to 1 GHz, and can include dual Ethernet, and LCD parallel interface STM32MP13 includes 3 different lines, which are pin- | |
![]() | Digi ConnectCore® 93 SoM Digi ConnectCore® 93 is a wireless, highly power-efficient and secure system-on-module based on the NXP i.MX 93 processor. It offers flexible connectivity with integrated 802.11ax dual-band Wi-Fi 6 and Bluetooth® 5.2, and integrates an AI/ML NPU. The | |
![]() | Digi ConnectCore® MP1 SoMs Digi ConnectCore MP1 System-on-Modules recognized as industry’s smallest STM32MP1 wireless SOM, reducing development risk and accelerating time-to-market for transportation, medical, and industrial applications. Key features Scalability and perf |
Article
Network Transformation: Taking Security to the edge
The ongoing digitisation of the workplace and the rise of the distributed workforce is forcing companies to redefine the security of their IT infrastructure.

Literature
Secure Provisioning Capabilities
Main stake of IoT Security - IoT Security implies the use of good practices in term of products, developments but it implies also to reduce opened doors, and provisioning is one of them.

Article Series
The IoT Security Series
Read our series of IoT security articles, put together by our in-house IoT, Connectivity and Wireless experts. Find articles and resources on device provisioning, network architecture, device authentication, lifecycle management and much more.

Article
Interview Thomas Pilz: Cyberattack victim - Fight like Rocky!
Thomas Pilz, CEO of Pilz Automation talked with Smart Industry about how it feels to be a cyberattack victim and what he thinks is the best way to defend against cybercriminals.

Literature
IoT security considerations checklist
To help you get started, we’ve created an essential checklist of the questions you’ll need to consider before deciding whether to go alone and build an internal team to execute IoT solution, outsource or work with a technology solutions provider.

Article
IoT Security: Identity of things
The more you have, the more you get: identity plays a key role in securing IoT, and the number of digital identities to manage tends to grow exponentially – many more than existing identity and access management (IAM) systems need to support.

Whitepaper
IoT security - real problems and solutions
This paper aims at defining the real issues and challenges behind IoT security, from hardware and embedded to server software, in advance of IPv6 and 6LoWPAN.

Article
Standardization Risk Management: How Much Cybersecurity Is Enough?
There’s no doubt that cybersecurity is a complex topic to legislate. Given how fast-moving security’s components are, legislation is often too slow and cumbersome.

Solutions
Internet of Things
Avnet Silica has the perfect supplier offering to enable you to put your product development into the Internet of Things.

Training & Events
Learning for better, faster projects builds
Connect with the Avnet Silica experts who will guide you to reach further with your projects with on-going seminars, workshops, trade shows and online training.

Avnet Silica
LoRaWAN Security Solutions
The TO136 is Avnet Silica’s exclusive secure element. It is manufactured on a hardware base supplied by Morpho and is loaded with a firmware developed by Trusted Objects and personalized with unique keys and IDs in a secure area.

Contact us
Have a question?
Do you have any questions about Security solutions offered by Avnet Silica? Then please feel free to contact our experts at security-solutions@avnet.eu.