Custom Meta Tags
Hero Banner Security Series
Sub Navigation
Main title (LC)

Device Lifecycles: Managing IoT Devices from Birth to Renewal

Title (LC)

Conceptually, the IoT comprises large numbers of devices connected to the internet, collectively capturing and reporting huge quantities of data to contribute to larger man-made goals, without direct human intervention. As a system containing many parts, proper management of each throughout its lifecycle is essential to ensure the system’s reliability and longevity. Moreover, because this is the IoT, lifecycle management is also critical to ensure security.

Introduction cont (MM)

To address each of these aspects, device lifecycle management should begin at the initial design and manufacturing stage and extend to cover procurement and distribution, configuration and connection, operation, and eventual decommissioning. The lifecycle of IoT devices can be described in five stages (Figure 1).

Design and Manufacturing

For the most part, typical embedded-systems design principles apply. However, designing IoT devices demands special focus on aspects such as connectivity, interoperability, regulatory compliance – to ensure adherence to standards regarding data protection and privacy – and, of course, security.

Main body (LC)

Device lifecycle stages

Figure 1: The device lifecycle process

With IoT devices, perhaps more than any other category, the phrase “baked in” has become synonymous with the approach required to ensuring each individual unit can be kept secure from the time it is manufactured to its end of life. Its meaning is that security should not be considered as an afterthought or an add-on feature but instead must be an integral part of the device's architecture and functionality. It begins with a secure-by-design approach that pays proper attention to security threats and effective defences from the early stages of development. This includes incorporating security features, implementing secure protocols, and conducting threat modelling and risk assessments.

Hardware-based security, leveraging components such as embedded secure elements (eSE) or trusted platform modules (TPMs), provides secure storage of cryptographic keys and credentials such as device identity, as well protecting boot processes and facilitating secure communication. In addition to benefiting from immutability, reliance on hardware components also overcomes the shortage of processing power, typical in IoT devices, that often prevents using complex software security algorithms.

Embedded security also encompasses the use of strong encryption protocols, such as Transport Layer Security (TLS), to ensure secure communication with other devices and backend systems.

Protecting firmware and software calls for the use of secure coding practices, with regular security testing and code reviews. Vulnerabilities must be swiftly addressed through patches and updates. It is also important to minimise device attack surfaces, by analysing and designing-out possible entry points or vulnerabilities and using secure memory management and input validation.

A mechanism for regular, secure firmware updates is also essential, to address security vulnerabilities and patch any security flaws. This usually requires a secure method for distribution and installation, such as over-the-air (OTA) updating with on-device firmware to check the authenticity and integrity of the code. Best practice is to check the code when the update is received and as part of secure boot-up each time the device restarts.

Supply-Chain Management

A comprehensive approach to device lifecycle management should also encompass supply-chain aspects such as the procurement of devices and testing against the specifications and standards for each, as well as logistics and distribution. This includes delivering IoT devices to various locations for deployment. As with manufacturing any other electronic devices, maintaining vendor relationships, quality control, and inventory management to avoid stock outages or excess inventory are important aspects of device management. Maintaining high standards of quality control prevents faulty or defective products reaching the market and ensures that IoT devices meet the specified standards.

Underlying everything, protecting the IoT devices and the data they contain – including intellectual property and any security credentials loaded at the time of manufacture - against malicious interference is extremely important throughout the entire supply chain.

One aspect that must be accounted for is unauthorized production. As an OEM, you typically want to be monitoring the actual number of devices that are effectively manufactured by your contracted partners. Making sure that the device is imprinted with a digital identity for which you or someone you trust controls the issuance is blocking unauthorized production attempts.

IoT Support (CO)

We understand that the IoT can be overwhelming, so if you need support with your next IoT project or IoT security in particular, why not get in touch with our experts? Our IoT, Wireless and Connectivity teams are on hand to help you with your next IoT challenge.

Learn More
Secure Provisioning (GBD)

Security

Secure Provisioning

Services providing keys and certificate injection into Secure Elements or MCU for full end-to-end Security.

Main body and conclusion (LC)

Finally, the OEM should also ensure secure firmware installation, meaning the capability to be certain that only the desired piece of software has been installed on the device, and in some cases making sure that this operation can be done while preserving the confidentiality of that piece of software during the operation. This is implemented using similar technologies than in the context of secure firmware update, but the initial installation is absolutely required as it is one of the crucial steps in maintaining trust in the device state.

Deployment and Provisioning

When managing the initial deployment of new devices to the network, it is important that settings are correctly configured for specific use cases or environments. Provisioning ensures that devices in the system are properly prepared to communicate securely, exchange data with other devices or the cloud, and perform their intended functions within the larger IoT ecosystem. The counterpart on the cloud infrastructure is to make sure that it is also configured to authenticate these devices and communicate with them in a secure way. This entails the registration of Certificate Authorities in the system, or whitelisting (and potentially blacklisting) certificates, or a combination of both.

Operational management

IoT devices need to be managed continuously, to perform the expected operational tasks for the duration of their expected lifetime. Monitoring device health, performance, and operational status on an ongoing basis allows the system to optimise the device settings and respond to events such as premature device failure or malicious damage. Monitoring can be achieved by analysing sensor data or by other means such as tracking connectivity statistics and power consumption, or by monitoring the device’s own diagnostic signals if available. In cases where device issues can be detected remotely, remote troubleshooting may also be possible, such as restoring settings or forcibly restarting the device.

Managing and deploying firmware updates, security patches, bug fixes, and feature enhancements is an essential part of device management, needed to keep devices up to date and secure.

Retirement and Decommissioning

Planning for the end-of-life phase of IoT devices is critical and can affect security as well as the environment. Poor disposal practices or simply leaving devices unguarded in the field at end-of-life creates risks such as data leakage and security vulnerabilities. If devices can be stolen or taken over, malicious actors may be able to recover sensitive information from the device. They may try to use stored credentials to gain unauthorised access to the host network.

Proper handling of data on retired IoT devices is essential and several relevant standards provide recommendations. These include ISO/IEC 27001, which offers a framework for information security management, including guidelines for disposal of media and equipment. The US security standard NIST SP 800-53 also has guidelines for secure data disposal, media sanitisation, and decommissioning of information systems.

Conclusion

Effective IoT device lifecycle management encompasses the strategic planning and coordination of activities across the entire lifespan of devices, from design and manufacturing, through operational management and maintenance during the normal lifetime, to retirement. Properly handling the end-of-life phase of IoT devices is essential to mitigate risks with data leakage and minimise security vulnerabilities as well as environmental impact.

This article closes the first part of this series that was focusing on the core concepts of identification, authentication, authorization, and life cycle management. The next articles will cover the different level of architecture involved into a typical IoT use case, from the devices to the network to the cloud infrastructure itself.

More from this series:

IoT Security Authors (LC)

About Author

 

Author placeholder image
EMEA IoT Security Experts

We use 'EMEA IoT Security Experts' as a collective byline when our team of IoT Security experts and writers collaborate on content.

 

PDF article pages (MM)

All IoT Security articles in one place...

What happens when the devices we depend on become our greatest vulnerabilities? As the Internet of Things (IoT) continues to surge in both range and frequency of use, with billions of devices connecting our homes, workplaces, and cities, the same technologies that make our lives more efficient also introduce unprecedented risks. Securing this intricate web of communication isn’t just a technical challenge — it’s a matter of trust, safety, and resilience in an increasingly connected world.

Download the full PDF today to access all of our IoT Security Series articles in one place for convenience and read them at a time that suits you. This PDF also includes an overview of the current state of IoT security and what to expect in the next decade.

IoT Security Series PDF front cover
PDF download (MFUR)

Fill in the short form below to start your PDF download.

 
Your download will start in {seconds} second(s). If your download doesn't start <a href="{url}" target="_blank">click here</a> to download.
 
Secure elements (GBD)

Security

Secure Elements

Hardware Root of Trust used for crypto operations and key storage.

Secure Library (GBD)

Security

Secure Library

Software Root of Trust integrated into any MCU/MPU used for crypto operations and key storage.

Secure MCU (GBD)

Security

Secure MCU

MCU with built in security features and key storage.

IoT Overview (GBD)

Service

See IoTConnect

The IoT can be overwhelming. You need to leverage new technologies like AI, deep learning and data mining to make the most of your investment. Let us help you.