Custom Meta Tags
Hero Banner
Power applications (SubNav)
SiC shines a light on solar power - Main Title (MT)

SiC Shines a Light on Solar Power

Introduction (MM)

Worldwide electricity consumption is growing fast, expected to rise by circa 4% annually from now to 2027. Solar photo voltaic (PV) generation is forecast to provide about half of this extra electricity, driven by falling PV prices and the need for zero-emission power.

Global solar PV capacity has already tripled from 2018 to 2023, reaching over 1,600 TWh. This trend is accelerating, with strong growth particularly in China, supported by the USA, the European Union and India – and is in line with what is needed for our planet to hit the target of Net Zero emissions by 2050.

Solar photo voltaic technology steps up

Solar panels with flowers in the forefront
Main copy (LC)

LOOKING FOR SUPPORT? CONTACT OUR POWER EXPERTS

The technology of solar power generation has improved steadily year-on-year, while prices have fallen dramatically. Solar PV is also a scalable technology that can be manufactured in high volumes, enabling rapid deployment and economies of scale.

Manufacturers are continuing to invest heavily in developing more efficient PV technology, enabling solar cells to capture more of the sun’s energy. While the market has been dominated by passivated emitter and rear contact (PERC) and passivated emitter, rear totally-diffused (PERT) panels, the industry is shifting to the newer, tunnel oxide passivated contact (TOPCon) technology, which promises higher efficiency at a competitive cost.

As well as the panels themselves, it’s vital that all the power electronics involved in solar energy generation are as efficient as possible. The key component is the inverter, which takes the DC generated by the solar panels and converts it to AC that can be fed back to the grid or used to drive local loads.

Research is focussed on improving inverter efficiency, as well as developing smarter inverters that integrate with a smart grid: to help balance supply and demand, and to handle ‘Dunkelflaute’ events when the wind doesn’t blow and the sun doesn’t shine.

Wide bandgap efficiencies in solar PV systems

An inverter in a solar PV system is based around a switching power device, which has traditionally meant a silicon MOSFET or IGBT. Over the years, there have been continued improvements in these devices, but the industry is now reaching the physical limits of silicon as a material – which means that to further improve efficiency, we need to look elsewhere.

The answer is silicon carbide (SiC), a wide bandgap (WBG) semiconductor that has some key advantages over silicon. Most importantly, SiC can switch faster than silicon, reducing switching losses and thus improving efficiency in power conversion devices such as an inverter. SiC MOSFETs deliver lower turn-on, turn-off, and conduction losses than equivalent silicon MOSFETs, which means their overall losses are over 60% lower.

SiC devices can also handle higher temperatures and voltages better than silicon, and have superior thermal properties, enabling them to dissipate heat more effectively. Additionally, SiC’s higher efficiency means it generates less waste heat than silicon, so heat sinks can be smaller, reducing overall equipment size and decreasing cost.

For small-scale solar PV systems, such as on homes and commercial buildings, another good option, in theory, is gallium nitride (GaN). This would provide higher switching speeds again, such as up to circa 300 kHz in a solar inverter application. The higher frequencies mean that output filters can be smaller, leading to a more compact design with higher efficiency than silicon.

SiC a clear winner by the numbers (LC)

SiC: a clear winner by the numbers?

Improved technology is all very well, but can we quantify how much of a difference SiC’s improved efficiency actually makes in solar power generation?

According to PECTA, a typical SiC-based PV inverter can achieve peak efficiency of somewhere between 98.2 to 99.2%, depending on the device used amongst other factors. PECTA chose a commercially-available converter with a peak efficiency of 99.2% for its calculations, and worked out that this would provide an efficiency improvement of approximately 2%, compared to existing silicon-based alternatives. Other estimates are for savings of less than 2%, for example the US Department of Energy suggests a 1% figure, but there is a consensus that SiC will deliver substantial efficiency gains.

Taking the 2023 figure of global solar PV generation capacity mentioned earlier (1,600 TWh), this 2% efficiency improvement would result in an extra 33 TWh of clean electricity being available per year. That’s about the same as the total electricity production of Denmark or Ireland, for example. To put it in terms of reducing CO2 emissions, it is approximately equivalent to taking 4 million petrol or diesel cars off the road.

Lighting the path to Net Zero emissions

Avnet Silica and its power semiconductor suppliers can provide the technologies, products and expertise you need to achieve efficient, reliable solar power systems.

From a full range of power switches including IGBTs, SiC MOSFETs and diodes to modular solutions for inverters and other functions – whatever your solar energy application, talk to Avnet Silica’s experts to find out how we can help you.

Spot Power (GBL)

Technology

Power: designing solutions with power at the core

We provide you with the right insights and expertise when you need it most, so you can make the right decisions for your product, and your business.

Power - Power components lighting up on board
EM (CO)

Avnet Silica is involved with every facet of the energy transformation and no matter what you’re designing, our experience and broad offering will ensure your application is fully charged for success.

ENERGY MANAGEMENT
Working on a project (LC)

Working on a power project?

Our experts bring insights that extend beyond the datasheet, availability and price. The combined experience contained within our network covers thousands of projects across different customers, markets, regions and technologies. We will pull together the right team from our collective expertise to focus on your application, providing valuable ideas and recommendations to improve your product and accelerate its journey from the initial concept out into the world.

WE'D LOVE TO HEAR FROM YOU!

Follow us (GBL)

Like what you see?

Follow us on LinkedIn

Follow our dedicated power page on LinkedIn for the latest power updates and news from our team of power experts.

Modal
Contact us

Submit your inquiry via the form below.