Custom Meta Tags
Hero Banner
Wide Bandgap (SubNav)
Title and intro (LC)

Five Things to Consider Before Switching to SiC in Power Conversion

SiC MOSFETs are often presented as an attractive upgrade to older technologies such as IGBTs and Silicon MOSFETs. Although in some limited cases, SiC can be a drop-in replacement, to get maximum benefit, the system should be considered as a whole. To explain more, the Avnet Silica Power Specialists discuss five example areas which affect your design approach. 

Gate drivers (MM)

1. Does the Gate Driver Change?  

Practically, yes. Although drive voltages are similar to IGBTs and Si-MOSFETs, optimum values are different and absolute maximum levels are typically lower. Even if an existing driver voltage swing is acceptable, perhaps +18V/-5V, edge rates also have to be ultra-fast to take advantage of the speed of a SiC MOSFET. Rates must still be controlled though, as the high dV/dt and di/dt levels can cause gate ringing, damaging overshoots and unacceptable EMI. Control is often implemented by arrangements of series resistors and diode gating to achieve different edge rates of positive and negative transitions. Some manufacturers recommend a series bead inductor to slow edges, but this must be adequately damped to avoid ringing with the gate capacitance. The absence of ringing in an existing gate driver for an IGBT or Si-MOSFET is no guarantee it won’t occur with a SiC device, as its gate dynamic characteristics are quite different, due to far lower internal capacitances. Some drivers [1] will include an external parallel gate resistor Rgs and capacitor Cgs to stabilise these values. As one example, Nexperia’s SiC MOSFETs are designed to optimise gate control, ensuring efficient and reliable switching performance in demanding applications.

LOOKING FOR SUPPORT? CONTACT OUR POWER EXPERTS

Schematic_SiC-FET-gate-drive
An example SiC MOSFET driver arrangement (Source: ROHM)
Main body (LC)

2. Will it Impact the Rest of My Design?  

Here you have a choice. If you are upgrading an existing design that’s using IGBTs or Si-MOSFETs, just doing the swap and updating the gate driver as described will usually get the design up and running. This can give a useful system efficiency boost with the potential to reduce heatsinking, but there will probably be a net component cost increase. A ground-up new design would consider increasing switching frequency to gain further advantages, such as smaller passives and improved system dynamic response to load changes. However, these advantages are offset by a possible increase in dynamic losses at the higher switching rate. 

3. Do I Really Need High-Frequency Switching?  

A headline characteristic of SiC is its potential to switch at high frequency. However, the corresponding increase in switching losses in ‘hard-switched’ conversion topologies may be unworkable, forcing a change to ‘soft-switched’ or resonant arrangements. These are generally more complex and can have limitations, such as trading lower dynamic for higher static losses for a given power transfer. A good reason to increase switching frequency is to reduce the size and cost of magnetics. However, in some applications such as motor drives, the magnetic element is the motor itself, which is sized for the power it delivers, so this advantage is not present. For this reason, many motor drives still operate around 10kHz and here, the low conduction losses, high voltage capability, ruggedness and low cost of IGBTs are still attractive. If a frequency ‘sweet spot’ is found where a SiC device has total lower dynamic and conduction losses than an IGBT in a motor drive, in an industrial environment for example, the energy saved may still be minor compared with the value for the load. The motor driver can be smaller though, which is a benefit. However, with advancements in SiC technology from suppliers like Nexperia, designers now have access to MOSFETs that balance conduction and switching losses to deliver a compelling alternative.

4. How Will it Impact My Passives? 

To get the most benefit, any efficiency increase achieved can be leveraged by reducing power converter heatsinking size, weight and cost while maintaining safe junction temperatures. Alternatively, for the same heatsinking and die size, junction temperatures are lower and reliability higher. In practice, SiC die sizes are smaller than IGBTS for the same headline ratings so junction temperatures can actually be higher, and although SiC as a material can stand much higher temperatures than Si, the limit is practically set by device packaging. By utilizing SiC, it might be possible to eliminate heatsinking completely, or cooling air dramatically reduced. If an increased switching frequency is considered, magnetics can be reduced in size, with weight and cost savings. Usually, capacitor values can be reduced at higher switching frequencies, such as in input and output filtering, for further economies. In some cases, the reduced capacitor values allow higher-performance ceramic types rather than electrolytics with their limited lifetime. 

5. Do I Need to Choose Parts with Top-Side Cooling?  

The highest efficiency converter designs with SiC will use SMT devices rather than through-hole, to help avoid problems seen with the parasitic inductances of leaded parts. The efficiency gains achieved with SiC might allow heatsinking through the circuit board copper layers, possibly onto a bottom-side heatsink, but if the heat generated is too high, top-side cooled SiC devices are available. This can free up PCB area, provide very low thermal impedance, allow more flexibility in board design and match in with automated assembly techniques. 

A top-side cooled device (Source: STMicroelectronics)

A top-side cooled device (Source: STMicroelectronics) 

Conclusion 

All power designs are a trade-off between performance, efficiency, size, weight and cost. Depending on the application, the starting point for a design decision tree will be one or more of these factors. For a new design, a SiC MOSFET approach can give an excellent overall solution. The Avnet Silica Power Specialists can suggest solutions, and with their expertise, help you to make informed design decisions. 

Reference

[1] Rohm – SiC MOSFET Basics and Design Guidelines for Gate Drive Circuits

Working on a project (LC)

Working on a power project?

Our experts bring insights that extend beyond the datasheet, availability and price. The combined experience contained within our network covers thousands of projects across different customers, markets, regions and technologies. We will pull together the right team from our collective expertise to focus on your application, providing valuable ideas and recommendations to improve your product and accelerate its journey from the initial concept out into the world.

WE'D LOVE TO HEAR FROM YOU!

Spot Power (GBL)

Technology

Power: designing solutions with power at the core

We provide you with the right insights and expertise when you need it most, so you can make the right decisions for your product, and your business.

Power - Power components lighting up on board
WBG (CO)

With the ongoing shift to renewable energy and the electrification of transport and industry, the demand for higher power and greater energy efficiency in electronics is increasing. Wide bandgap technologies including SiC and GaN bring many advantages.

WBG OVERVIEW
EMEA Power Experts (LC)

About Author

 

Author placeholder image
EMEA Power Experts

We use 'EMEA Power Experts' as a collective byline when our team of power experts and writers collaborate on content.

 

Follow us (GBL)

Like what you see?

Follow us on LinkedIn

Follow our dedicated power page on LinkedIn for the latest power updates and news from our team of power experts.

Modal
Contact us

Submit your inquiry via the form below.