Custom Meta Tags
Hero Banner
Power applications (SubNav)
Global emissions (MT)

Global Emissions, Swept Away by Wind Power

Introduction (MM)

To meet global goals for emissions reductions, we need to generate more electricity from renewables – and lots of it. Solar photo voltaic (PV) systems may be the centre of attention, but wind power is also a vital contributor to our push towards net zero.

How is progress in the wind power generation industry? And what can the power electronics sector do to help us hit our targets?

LOOKING FOR SUPPORT? CONTACT OUR POWER EXPERTS

Wind power progress: are we on track?

Wind turbines on top of hill
Global emissions main copy (LC)

In 2023, the world’s cumulative installed wind power capacity passed the 1 TW (1,000 GW) landmark for the first time. It was a record year, with 113 GW of new wind power capacity connected to power grids, the majority in China (76 GW). There are now ten countries which generate more than 20% of their electricity from wind power.

The demand for wind energy continues to grow rapidly, from 8% of global electricity generation in 2023 to a predicted 14% in 2030, according to the IEA. While there are economic, regulatory and supply chain challenges to overcome, investment in wind is strong around the world, and ambitious targets are looking achievable.

The key to efficient power conversion

Power conversion is required in a wind turbine, since it typically generates variable frequency alternating current (AC) electricity, which is first rectified to direct current (DC), and then subsequently converted to high voltage AC at a frequency and voltage compatible with the grid.  

It’s a booming sector – according to Yole Intelligence, the market for power converters for wind power will grow at a compound annual growth rate (CAGR) of 10.4% from 2022 to 2028.

To maximise their output of useful energy, wind power systems need this power conversion to be as efficient as possible. To achieve this, there is an increasing shift to use wide bandgap (WBG) power semiconductors to handle switching in the turbine’s inverter, rather than the traditional silicon IGBTs.

While silicon has been the material of choice for switching in inverters for decades, its limits are now being reached – and Wide Bandgap devices are taking up the mantle of the drive towards ever-higher efficiency.

SiC vs IGBT in wind power

The two most commonly-used WBG semiconductor materials are silicon carbide (SiC) and gallium nitride (GaN). They both provide fast switching and excellent efficiency, but SiC is often a better choice for wind power.

Why is SiC preferred? It provides the capability to operate at high voltages and high temperatures, making it an excellent fit for use in wind turbines. This is particularly true in large, utility-scale installations where voltages are typically above 1000 V.

SiC-based devices reduce switching losses in the inverter, compared to silicon IGBTs. SiC also provides lower turn-on, turn-off, and conduction losses than silicon. The losses experienced, and their relative size, do depend on the load on the power converter, which in turn depends on the wind’s speed. By varying the switching frequency as a function of wind speed, efficiency at low loads can be maximised.

Spot Power (GBL)

Technology

Power: designing solutions with power at the core

We provide you with the right insights and expertise when you need it most, so you can make the right decisions for your product, and your business.

Power - Power components lighting up on board
SiC vs IGBT (LC)

Taking all losses together, SiC MOSFETs can typically achieve more than 60% lower losses than an equivalent silicon IGBT device. In research by Norwegian University of Science and Technology, at switching frequencies of around 5 kHz, a solution based on SiC MOSFETs offered around 1% improved efficiency, compared to using silicon IGBTs – which may sound small, but is highly significant over a system’s lifetime.

With lower power losses meaning less heat is dissipated, and the better thermal performance of SiC, the thermal management of an inverter can be improved with SiC. This means that reliability can be improved, thus extending turbine lifespan and reducing the cost of maintenance – especially important in hard-to-reach offshore locations.

Analysis at the University of Nottingham showed that the move to SiC achieved a one-third reduction in heatsink volume, thus enabling the cooling fan to be discarded. The analysis also showed that using SiC MOSFETs enabled a reduction in the size of passive components used in the power converter, thus helping to further shrink the system size.

SiC does still have some barriers to adoption, not least that it requires system redesign to obtain best results, meaning there is a learning curve for design engineers. The higher switching frequencies of SiC-based systems can also create new challenges in managing EMC issues, with an impact on PCB layout.

And while there is an increasing number of SiC MOSFETs available from multiple suppliers, they are still more expensive than the equivalent silicon devices – although this cost differential is shrinking year-on-year.

Conclusions

With a wide range of SiC and GaN devices available, Avnet Silica’s power semiconductor portfolio supports the future of wind power. Talk to our experts today to find out how we can help you.

Working on a project (LC)

Working on a power project?

Our experts bring insights that extend beyond the datasheet, availability and price. The combined experience contained within our network covers thousands of projects across different customers, markets, regions and technologies. We will pull together the right team from our collective expertise to focus on your application, providing valuable ideas and recommendations to improve your product and accelerate its journey from the initial concept out into the world.

WE'D LOVE TO HEAR FROM YOU!

Featured podcast (LC)

Featured podcast


Episode 37: Unleashing the Power of Wind Energy


Hold on to your hats: In today’s episode, we discuss one of the fastest-growing renewable power sources: wind energy. Did you know that a single wind turbine has the potential to generate enough electricity to power 1,400 homes?

In this episode, we welcome Barry Thompson, CEO of Alpha 311.

We'll unpack how cutting-edge technologies and ingenious strategies are evolving in this sector, emphasizing the impact of IoT in enhancing turbine efficiency. Our discussion will also cover the ecological benefits of wind power and a forward-looking perspective on this form of renewable energy.


Follow us (GBL)

Like what you see?

Follow us on LinkedIn

Follow our dedicated power page on LinkedIn for the latest power updates and news from our team of power experts.

Modal
Contact us

Submit your inquiry via the form below.