Industry 4.0 is changing the way in which manufacturing facilities and processing plants operate. Through the acquisition and subsequent analysis of data, workflows and process parameters can be changed in order to raise efficiency levels, ramp up output and improve end product quality. The increased pervasiveness of automation is leading to smart factories that are much less dependent on human resources. This translates into lower operational expenses, heightened productivity, as equipment can run 24/7, and less chance that errors could impact on yield or result in product returns.
Working with EBV, you will be better able to identify and leverage key industrial applications. Our specialists help you see the big picture and target the areas with the strongest potential for success – from production safety to automation, from miniaturisation to connectivity and beyond.

Let's talk
Better connected through LinkedIn
Get directly in touch with our Industrial Director Karl Lehnhoff

A new age of visibility
With the large-scale deployment of Industrial Internet of Things (IIoT) devices throughout industrial sites, the performance of the numerous constituent elements can be continuously monitored to a high degree of granularity. This will ensure that everything is running correctly and flag any issues to be addressed so that it does not lead to inferior products, create additional wastage, or cause machinery to be damaged. This monitoring data can also be of value in preventing potentially catastrophic events occurring, where the lives of the workforce could otherwise be endangered. Any problem that might emerge can be identified at an earlier stage, before the situation has become too serious.
Closer cooperation between humans and robots
Robots and automated guided vehicles (AGVs) are becoming more commonplace in warehouses and on factory floors. Though in the past robotic arms would be operating in heavily restricted areas, robots are now being expected to work alongside human staff - generally being referred to as collaborative robots (or cobots). This means that their movements need to be much better controlled through high precision motion sensors and the imaging data provided by on-board cameras. Higher accuracy location data is also required, being determined via UWB or GNSS.
Detailed modelling of industrial operations
The digital transformation now underway is set to enable predictive maintenance to be undertaken. Studying captured datasets will mean that component parts that need replacing can be pinpointed before they wear out or stop functioning. Consequently, unwanted disruption and costly downtime will be avoided. By taking the data derived from items of complex equipment, it is now possible to generate highly detailed virtual approximations of their original physical forms. Using such ‘digital twins’, the longer-term effects of different operational scenarios can be played out to check their validity - such as increasing the speed or the temperature levels that equipment is running at, using different raw materials. This can be done at a greatly accelerated rate, so that projected outcomes more than a decade ahead may be seen. As all this is happening in the virtual domain, rather than in the real world, there is no risk of the equipment being broken or workers being harmed.
Overcoming communication challenges
New factory installations will generally roll out multi-Gbit Ethernet networking infrastructure to support their data transmissions. However, a large proportion of existing industrial operations will have older machinery that utilises outdated fieldbus protocols or even proprietary protocols that are incompatible with modern communication standards. As it will usually represent too large an investment to dispose of all this machinery, alternative methods are needed. Legacy items can easily be upgraded by retrofitting them with wireless modules. These modules can be arranged in mesh, star, ring or tree topologies, as application requirements dictate.
LPWAN wireless solutions are being employed in a lot of industrial use cases. Though the advent of 5G mobile, due to the faster data rates and low latency capabilities it offers, seems likely to encourage the establishing of private networks at many industrial and logistics sites. It is of course, paramount that the data being carried over wireless networks, whichever protocol or standard is chosen, does not become compromised, with malicious third parties prevented from accessing it. Therefore stringent security mechanisms need to be put in place.
Related technical articles
Why EBV?
EBV Elektronik is widely regarded as the foremost distributor of electronic components for the industrial sector. The core industrial franchises we partner with are AMD, ams OSRAM Group, Broadcom, EBV Chips, Infineon, ISSI, Microchip, Micron, Nexperia, NXP, onsemi, Power Integrations, Renesas, Samsung, SGMICRO, SIMcom, STMicroelectronics, Toshiba, Tria and Vishay.
We can provide the various sensors needed for industrial monitoring, enabling data on all different types of operational parameters to be measured. In addition, we offer access to a broad range of imaging solutions for machine vision applications, plus motor driver ICs and motion control solutions. Our industrial networking portfolio covers both wireline and wireless communication - with Ethernet, LPWAN and cellular IoT related ICs and modules all being available. On top of this, there are industrial MCUs and memories, as well as the latest security chips. Finally, we have SoCs, FPGAs and displays that can form the basis for human machine interfaces (HMIs) via which workers will be able to interact with machinery.

Infineon Memories for Embedded Systems
When failure is not an option, depend on our broad portfolio of high-performance memory solutions for automotive, industrial, and communications applications.

Infineon General-Purpose MOSFETs
Infineon strives to serve all customers by offering power MOSFETs meeting any of your design, pricing, and logistical requirements.

Infineon Memory Solutions
Infineon offers the broadest portfolio of Flash and RAM solutions designed specifically for industrial and communications applications.

onsemi RSL10 Smart Shot Camera Solution
The RSL10 Smart Shot Camera platform integrates everything you need to put smart image capture at the edge of your network. Get years of active use out of battery-powered cameras that send data straight to your cloud platform.

Xilinx and onsemi Machine Vision Solutions
Choosing the right technology partners like EBV, Xilinx and onsemi for your next machine vision innovation optimizes efficiency, mitigates potential risks and maximizes profit potential.

Xilinx Acceleration Solutions for Software Developers
Vitis™ Unified Software Platform (Vitis USP) is created to simplify the development of highly optimized hardware-accelerated applications on programmable Xilinx platforms, including FPGAs, SoCs MPSoCs, and Versal ACAPs.
Resources
EBV Podcast
Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.


Broadcom Going Green
Broadcom optocouplers are the ideal fit for an array of green applications ranging from solar and wind inverters, energy storage, automotive electric vehicles and charging and power supplies.

Nexperia industrial solutions
Nexperia supports trends in the industrial environment by securing interfaces, reducing the size of various apps while also increasing the power density.

EBV presents: ST Analog
STMicroelectronics offers a wide analog portfolio of general purpose and application specific products for Power & Energy Management, Motor Control, Factory Automation and Connectivity, all dedicated to these markets.

Analog & Power Management
The era of digitalisation is ever advancing, almost as if our world were solely represented and controlled by ones and zeros. Every physical variable – be it an audio signal, temperature, voltage – is an analog value.

Infineon CoolSiC™ MOSFETs and Diodes
Infineon's portfolio includes CoolSiC™ Schottky diodes, CoolSiC™ hybrid models, CoolSiC™ MOSFET modules and discretes, plus EiceDRIVER™ gate driver ICs for driving SiC devices.

ST Standard Products Make All The Difference!
ST brings to you one of the broadest range of industry-standard and drop-in replacements for the most popular general-purpose Analog ICs, Power Switches, Discretes and serial EEPROMs with thousands of references to help you optimize your supply base.
Do you have a question?
Contact EBV
If you need any assistance, please click below to find your closest EBV sales office.